Hello,
I followed steps as mentioned in "http://wiki.davincidsp.com/index.php?title=USB_File_Storage_Gadget".
With the DM355 EVM board I could see the EVM board being identified as a mass storage device on the Windows and Linux PC's.
I could access the the EVM boards as a mass storage device from Windows/Linux PC's.
I have a board based on DM355 processor. I tried the same procedure(infact the same kernel was used to test with EVM board) but the board does not get recognized as mass storage device.
On Windows machine a pop up comes "Unrecognized USB device".
Can any one point out what could be the issue ?
Thanks,
Snehal