This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS/AM5728: CCS Error after QSPI-boot with PROCESSOR-SDK-RTOS-AM57X

Guru 10235 points

Part Number: AM5728

Tool/software: TI-RTOS

Hello, TI Experts,

 

We have a question about QSPI-boot with TMDXIDK5728.

We successed to QSPI-boot based on below link.

http://processors.wiki.ti.com/index.php/Processor_SDK_RTOS_BOOT_AM57x#Booting_Via_QSPI

 

After that, we cannot connect A15 on CCS because of errors like below;

So, we tried to remove "gel file name" of Target Configuration file like attached pdf to avoid conflict of sbl board initialization in QSPI-flash.

(We think sbl in QSPI-flash has already the board initialization.)

Then we can connect A15 on CCS.

 

Question:

   Is this treatment for this CCS Error proper?

 

If there are any recommended way or notice for this problem, please tell us.

 

Best regards,

config.pdf