Part Number: TDA2EVM5777
Tool/software: Linux
HI,
I want to boot from emmc,Now I can find the emmc and write the boot files on it,How can I select the boot style on the TDA board?thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TDA2EVM5777
Tool/software: Linux
HI,
I want to boot from emmc,Now I can find the emmc and write the boot files on it,How can I select the boot style on the TDA board?thanks!
HI Yordan
I can start uboot from emmc,when i set sysboot as the link you gived,but the uboot can't read zImage and filesystem.
I used some commands to test ,like this:
=> load mmc 1:2 0x82000000 /boot/zImage
** File not found /boot/zImage **
=> ls mmc 1:2
<DIR> 4096 .
<DIR> 4096 ..
<DIR> 16384 lost+found
<DIR> 4096 bin
<DIR> 0 boot
<DIR> 0 dev
<DIR> 21 etc
<DIR> 0 home
<DIR> 0 include
<DIR> 0 lib
<DIR> 28 media
<DIR> 655 mnt
<DIR> 649 opt
<DIR> 5764 proc
<DIR> 4096 run
<DIR> 2668 sbin
<DIR> 224904 srv
<DIR> 110212 sys
<DIR> 129020 tmp
<DIR> 191052 Untitled Folder
<DIR> 0 usr
<DIR> 0 var
<DIR> 0 test_di
From above, uboot can recognize the filesystem,but can't read the file.
The files u-boot.img \ uenv.txt \ tisdk-rootfs-image-dra7xx-evm.tar.xz arm the same when I writed to SD card.
Hi,
Attached the uenv-emmc.txt file for your reference (please update the fdtfile argument according to the DTB you're using).
Regards
Shravan
fdtfile=dra71-evm-lcd-auo-g101evn01.0.dtb
rootfs=/dev/mmcblk0p2
args_mmc=part uuid mmc 0:2 uuid; setenv bootargs "console=ttyO0,115200n8 elevator=noop root=PARTUUID=${uuid} rw rootwait earlyprintk fixrtc omapdrm.num_crtc=2 consoleblank=0 cma=128M@0xB0000000 rootfstype=ext4 snd.slots_reserved=1,1"
HI ,I have resaved my problem,thanks , just because the tool mkfs.ext4 is too new.