Tool/software: Linux
Hello experts,
I am trying to load the uboot.img fie from the SPL and below is the error, i m facing
Not sure, whether it is problem of the SD Card reading or formating is not done.
U-Boot SPL 2017.01-g82ac813-dirty (Mar 11 2019 - 19:30:50) DRA722-GP ES2.1 boot device present boot device none boot device none boot device none boot device none Trying to boot from MMC1 i2c_write: error waiting for addr ACK (status=0x116) lp873x: could not set LDO1 voltage. reading logo.yuv reading am570x-mid.dtb spl_load_image_fat_os: error reading image args, err - -1 reading u-boot.img omap_hsmmc_send_cmd: timedout waiting on cmd inhibit to clear omap_hsmmc_send_cmd: timedout waiting on cmd inhibit to clear omap_hsmmc_send_cmd: timedout waiting on cmd inhibit to clear omap_hsmmc_send_cmd: timedout waiting on cmd inhibit to clear omap_hsmmc_send_cmd: timedout waiting on cmd inhibit to clear omap_hsmmc_send_cmd: timedout waiting on cmd inhibit to clear spl_load_image_fat: error reading image u-boot.img, err - -1 omap_hsmmc_send_cmd: timedout waiting on cmd inhibit to clear omap_hsmmc_send_cmd: timedout waiting on cmd inhibit to clear omap_hsmmc_send_cmd: timedout waiting on cmd inhibit to clear omap_hsmmc_send_cmd: timedout waiting on cmd inhibit to clear omap_hsmmc_send_cmd: timedout waiting on cmd inhibit to clear omap_hsmmc_send_cmd: timedout waiting on cmd inhibit to clear ** Can't read partition table on 0:0 ** spl: no partition table found omap_hsmmc_send_cmd: timedout waiting on cmd inhibit to clear omap_hsmmc_send_cmd: timedout waiting on cmd inhibit to clear omap_hsmmc_send_cmd: timedout waiting on cmd inhibit to clear omap_hsmmc_send_cmd: timedout waiting on cmd inhibit to clear omap_hsmmc_send_cmd: timedout waiting on cmd inhibit to clear omap_hsmmc_send_cmd: timedout waiting on cmd inhibit to clear ** Can't read partition table on 0:0 ** spl: no partition table found SPL: failed to boot from all boot devices ### ERROR ### Please RESET the board ###