Support,
Is there a limitation to resolution when using RFBI?
- TRM, section 13.1.1, shows RFBI 8/9/12/16 parallel interface (up to QVGA@30fps).
- Table 13-5 shows parallel RFBI with 16bit data.
- Does it support 8bit data
Want to interface to : HX8357, 320x480 dot, 16M color, TFT Single Chip Driver.
If supported, are there any drivers in the Linux SDK?
Regards,
Marc