Part Number: AM3352
Hello,
Currently we are using phyBOARD-Regor as our development hardware. This is compatible with Linux 4.4.52. As our application requires a RTOS to execute tasks. In regarding this, we are thinking to use, PROCESSOR-SDK-RTOS-AM335X. In regarding this we have few questions:
1. Can i boot the phyBOARD-Regor, by following the process mentioned in document PROCESSOR-SDK-RTOS-AM335X, Linux SD Card Creation Guide.
2. Can i install the Code composer studio(CCS) IDE in the phyBOARD-Regor itself and develop the application code (or) do I have to install the CCS IDE in Ubuntu 16.04 machine, cross compile the developed code as per ARM GCC and execute the executable after copying into phyBOARD-Regor.
3. Can i access the low level hardware of AM3352 with this SDK.
Thanks,
J. Chandra Sekhar