Part Number: TMDXICE110
Other Parts Discussed in Thread: AMIC110,
Hi , everyone,
I use TwinCAT to test EtherCAT by connecting AMIC110 ICE EVM(TMDXICE110), but it has "PREOP to SAFEOP failed" Error
As shown below
D7 red led will blink in AMIC110 ICE EVM when this error occur
- The following is my environment:
Windows 10 64-bit
TwinCAT 3.1 (3.1.4022.27)
CCS v8.3.0
pdk_am335x_1_0_13
PRU-ICSS-EtherCAT_Slave_01.00.07.02
pru_icss_ethercat_slave_prebuilt_01.00.07.02
processor_sdk_rtos_am335x_5_02_00_10
- Burning in file
| Binay Name | Flash Offset |
| C:\ti\pdk_am335x_1_0_13\packages\ti\starterware\binary\bootloader\bin\amic110-ddrless\gcc\bootloader_boot_mcspi_noDDR_a8host_release_ti.bin | 0x0 |
| C:\ti\PRU-ICSS-EtherCAT_Slave_01.00.07.02/protocols/ethercat_slave/ecat_appl/iceAM335x/tiesc_eeprom_ti.bin | 0x10000 |
| C:\ti\PRU-ICSS-EtherCAT_Slave_01.00.07.02/protocols/ethercat_slave/firmware/v1.0/ecat_host_interface_ti.bin | 0x14000 |
| C:\ti\PRU-ICSS-EtherCAT_Slave_01.00.07.02/protocols/ethercat_slave/firmware/v1.0/ecat_frame_handler_ti.bin | 0x19000 |
| C:\ti\pru_icss_ethercat_slave_prebuilt_01.00.07.02\applications\ethercat_slave_demo\AMIC11x\arm\AMIC11x_release\app | 0x20000 |
Where app I use from the pru_icss_ethercat_slave_prebuilt_01.00.07.02 , as shown in the last step of the above table.
Then copy C:\ti\PRU-ICSS-EtherCAT_Slave_01.00.07.02\protocols\ethercat_slave\ecat_appl\esi\TI_ESC.xml file to C:\TwinCAT\3.1\Config\Io\EtherCAT when using TwinCAT test
The error "PREOP to SAFEOP failed": Invalid SM IN cfg still occurs
How can I solve this problem?