Part Number: AM5728
Tool/software: Linux
Hai,
i am using am5728 custom board which is connected to windbond NOR flash memory through SPI interface. I want to partition the NOR flash memory using partition table
is it possible to create such table using any file formats like csv format which is then converted to binary format for flashing the table to NOR flash memory.
My requirement is, i should be able to update the partition table stored initially in flash memory after a period of time without compromising on-device software.
Thanks & Regards ,
R venkat