Part Number: AM3352
Hello Everyone,
We are using the AM3352ZCZ in our products with commercial temperature grade (Tj - 0°C to 90°C).
POH of the AM3352ZCZ is 100K for the junction temperature range: 0°C to 90°C for the following operation:
Processor is operated in turbo Mode (800MHz) and DDR3SDRAM is @ 400MHZ.
I would like to know that if the Junction temperature will go between 91°C to 110°C range which are the potential failures occurred to the system/processor?
Best Regards,
Karan Chauhan