Hi,
At the moment I'm working on a CPU board with custom DDR2 routing which we have implemented according to the datasheet (figure 7-39), one DDR2 device connected with 16 bit data bus width.
The DDR2 is functional and we are able to run firmware on it so it is stable, but when I measure the signals (with a MSO Tektronix scope and DDR2 analysis tools) I get a fail which I do not really understand.
The fail is about the Vswing(max) on CK(#) and DQS(#). in the JEDEC it is stated that is should be 1 Volt maximum but we use the DDR2 with 1V8 supply so we go over the requirement at least 0.5V and so the test is fail.
Is there any information/knowledge about this signal? The JEDEC does states it is a "test signal waveform", so do I need to enable test signals for DDR2 measurement?
Thank you for the support.