Part Number: TMS320C6657
Other Parts Discussed in Thread: TMDSEVM6657
Tool/software: TI-RTOS
Hello, Dear Friends. I have a problem with NDK to my project.
I am using next components:
-> bios_6_73_01_01
-> ndk_3_40_01_01
-> pdk_c665x_2_0_12
-> xdctools_3_51_01_18_core
What am i doing wrong? My code in attachment.
Source code:
#include <ti/sysbios/BIOS.h>
#include <ti/sysbios/knl/Clock.h>
#include <ti/ndk/inc/netmain.h>
#include "../h/knEthernetInit.h"
static const char *pIpAddr = "192.168.0.228";
static const char *pIpMask = "255.255.255.0";
static const char *pIpGateAddr = "0.0.0.0";
static const char *pHostName = "kotlin";
static const char *pDomainName = "kn.loc";
static void knNdkInitIp(void *pCfg);
static void knNetworkOpen(void);
static void knNetworkClose(void);
static void knNetworkIPAddr(uint32_t ipAddr, uint32_t ifIdx, uint32_t fAdd);
extern void llTimerTick();
void knInitEthernet(void)
{
extern volatile cregister Uns DNUM;
if ((1 << DNUM) & (1))
{
int resNc = -1;
void *pCfg = NULL;
ti_sysbios_knl_Clock_Params clockParams;
ti_sysbios_knl_Clock_Handle handle;
ti_sysbios_knl_Clock_Params_init(&clockParams);
clockParams.startFlag = TRUE;
clockParams.period = 100;
handle = ti_sysbios_knl_Clock_create(&llTimerTick, clockParams.period, &clockParams, NULL);
resNc = NC_SystemOpen(NC_PRIORITY_LOW, NC_OPMODE_INTERRUPT);
if(resNc)
{
while(1);
}
pCfg = CfgNew();
if (NULL != pCfg)
{
knNdkInitIp(pCfg);
do
{
resNc = NC_NetStart(pCfg, knNetworkOpen, knNetworkClose, knNetworkIPAddr);
} while(resNc > 0);
CfgFree(pCfg);
}
NC_SystemClose();
ti_sysbios_knl_Clock_delete(&(handle));
}
}
static void knNdkInitIp(void *pCfg)
{
CI_IPNET ipNet;
CI_ROUTE route;
CfgAddEntry(pCfg, CFGTAG_SYSINFO, CFGITEM_DHCP_HOSTNAME, 0, strlen(pHostName), (uint8_t *)pHostName, NULL);
memset(&(ipNet), 0, sizeof(CI_IPNET));
ipNet.IPAddr = inet_addr(pIpAddr);
ipNet.IPMask = inet_addr(pIpMask);
ipNet.NetType = 0;
if (strlen(pDomainName) < CFG_DOMAIN_MAX)
{
strcpy(ipNet.Domain, pDomainName);
}
CfgAddEntry(pCfg, CFGTAG_IPNET, 1, 0, sizeof(CI_IPNET), (uint8_t *)&(ipNet), NULL);
memset(&(route), 0, sizeof(CI_ROUTE));
route.IPDestAddr = 0;
route.IPDestMask = 0;
route.IPGateAddr = inet_addr(pIpGateAddr);
CfgAddEntry(pCfg, CFGTAG_ROUTE, 0, 0, sizeof(CI_ROUTE), (uint8_t *)&(route), NULL);
}
static void knNetworkOpen(void)
{
}
static void knNetworkClose(void)
{
}
static void knNetworkIPAddr(uint32_t ipAddr, uint32_t ifIdx, uint32_t fAdd)
{
}
Cfg file: