This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM4378: NAND flash compatibility check - ISSI IS34MW04G084

Part Number: AM4378

Using the GPMC interface, do you foresee any trouble using this NAND device? ISSI IS34MW04G084

Its specs all look compatible to me, but it is not an ONFI device (to the best of my knowledge).

Reading through the manufacturer's ID definition table and comparing with the AM437x Tech Ref Manual, I see some ID bits that don't quite match up between the two.

The chip's ID codes are (in hex):

Maker code: C8h

Device code: DCh

3rd byte: 90h

4th: 95h

5th: 54h

6th-8th: 7Fh

Thanks in advance