This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM3354: Daisy Chain Implementation using with EtherCat

Part Number: AM3354

Tool/software: Linux

Dear TI Team,

Currently in our custom board there is only one RMII interface available to be used. In "EtherCAT® on Sitara™ Processors" document it seems that it is  needed to use 2xEthernet PHY(Currently one pcs is available on our board. For the second one there is no restriction for us to use). And again in same document the interface which is used for ETHERCAT is MII. So Based on this we would like to kindly ask you the possibility of a daisy chain implementation with using EtherCat over one RMII.

 

Regards,

Zafer Çalışkan