This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/TDA2PXEVM: 4CH AVB surround view - add auto calibration

Part Number: TDA2PXEVM

Tool/software: Linux

Hi Sir,

My HW is TDA2x CPU board + Vision Board and SDK is PROCESSOR_SDK_VISION_03_05_00_00 with TDA2XX_EVM_LINUX_ALL define.

"AVB RX Usecases" and "Multi-Camera LVDS Usecases" both are working on my EVB,

but only "LVDS surround view case" has auto-calibration option, "AVB surround view case" has no calibration option.

Can I move "LVDS auto-calibration" function for AVB case using?

If yes, what's parameter structure and calculate link I have to modify after I move these structures and links to AVB use case?

Thanks.

Ranny.

  • Hi Ranny,

    You have to calibration manually.

    Please follow those documents:
    vision_sdk\docs\SurroundView\VisionSDK_UserGuide_3D_SurroundView_Manual_CalibTool.pdf
    vision_sdk\docs\SurroundView\VisionSDK_UserGuide_SurroundView_Calibration_TDA2xx.pdf

    Regards,
    Yordan