Hi everyone!
I'm working with DM355 to output digital video in the corresponding VPBE pins in BT.656 format. My intention is to output the video in 640x480 format, but as BT.656 is a fixed format I'm forced to put the useful video in a 720x480 frame. No matter about that. So far everything is ok.
I have some custom boards which are identical in hardware. I use the same software in all of them (this has been checked many times). The problem starts here: all the boards don't output the same video.
The "good ones" output the video shown in next image.

It is supposed to be approximately right: 640x480 useful video inside a 720x480 frame. The blue/purple vertical stripe is due to the unused space inside the video window (columns between 640 and 720). Sorry for the image quality as it is a photograph.
The "bad ones" output the next video.

I have no explanation for horizontal black stripe located at the bottom of the image. Besides, it seems that the rest of the image is kind of compressed. I mean, I can see more or less the same area than in a "good" board, but compressed in a smaller area.
Any idea why this is hapenning? Everything points to a hardware error on these boards, but I don't know what to think or where to start searching. I think I didn't say it but so far I tested 4 boards: 2 happened to be "good" and 2 happened to be "bad". So it doesn't look like an isolated error.
Thanks in advance!