This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

USB ID Pin



Hello,

 

Just wondering if I can get some clarification on the internal operation of the ID pin for the USB.  The datasheet only has a single line reguarding its operation.

We are trying to get the OTG functionality working and looking at the ID pin, it wants it either grounded or floating, but no pull up on the line.  It doesn't appear the is an internal pull-up either.  How does this actually end up working out, is there a very low voltage comparitor or what?  It seems strange because for normal device/host mode per the eval kits, you pull the line up/down.

Also, it implied that it looked at this pin to determine which mode to power up in, but the USB cable could potentially be plugged in and tie the ID pin to ground after the USB module is up and running, does the module need to be restarted?  If so, where/how can the ID pin be monitored, as I'm not seeing a register address to accesss the state of this input.

 

Thanks for any help you can give.

  • You are correct, USB_ID should be pulled up via 10K resistor.  USB_ID status is reflected in DEVCTL.BDEVICE register bit; see USB UG for more detaisl (http://focus.ti.com/general/docs/litabsmultiplefilelist.tsp?literatureNumber=sprued2c)

  • Juan,

     

    On the link you sent, it says "If using OTG or mini-USB connector, this pin will be set properly via the cable/connector configuration".  It doesn't say to pull up/down this line.  But the cable connects the ID pin to ground for host mode and leaves it floating for device mode.

     

    Further, the357 usb users guide (http://www.ti.com/litv/pdf/sprugh3) says the pin should be open or tied to ground via cable.

  • Mike,

    I do realize what the document suggests, but have verified with our factory team that indeed a small pull-up resistor is needed on USB_ID pin.  We will correct the documentation.  Also, I referred you to the doc more for the register settings, acknowledging the USB_ID pin suggestions are incorrect.  Thank you for your understanding.

  • Juan,

     

    Could I also suggest that a note be added to the USB User Guide describing that the state of the USB ID pin can be read from the DEVCTL.BDEVICE bit.  The only reference to the ID pin in that document is the pin description and the register itself just says that it tells what state the USB controller is in, not that is determined its state from the ID pin.

  • Mike, sure thing.  This sounds like a reasonable request.

  • Mike,

    I assume your are discussion about DaVinci USB Controller.  Can you specify which particular DaVinci Device are you refering to?

    The ID pin is used by the USB controller to determine the intented role that the controller has to switch to depending on the end of the cable that gets plugged into the USB connector.

    The fact that you are trying to test OTG the ID pin should be directly connected to the USB controller ID pin on the DaVinci device.  Pl. refer to the DVM schematics for the same.

    regards

    swami

  • I'm using the DM357.

     

    I do have the ID on the DM357 tied to the ID pin on the connector.  The issue is if the ID pin should be pulled up or left open as refered from the user guide.  Juan mentioned the documentation is in error and the ID should be pulled up via a 10k resistor.

  • Just to be clear, the value of the resistor is not strict, you need a small pull up resistor.  I have seen anywhere from 1.5K to 20K being suggested, but I know a customer that actually implemented this using a 10K, thus my recommendation.

    Remember that the USB ID pin is pin4 on the cable and this pin is either joined with pin5 (ground) or left unconnected (floating). The mini-A connector grounds the ID pin with Ground pin so that the ID Pin state is low. Up on seeing the state of the ID pin being low, the USB controller responds by assuming a Host role. If it is left floating, you need to have a weak pull-up so that the ID pin is High and the USB controller will respond by assuming the role of a Device.

  • Juan,

    I tried reading the BDEVICE register to see if the ID pin is pulled high or low, but it does not reflect the current state of the pin.  It does mention it is only valid when the session is valid.

     

    Is there any way to get the status of that pin without a session or somehow fool the controller into thinking there is a valid session so it will latch the state of the pin?

     

    Thanks,

     

    Mike

  • Mike,

    There is no need to monitor the ID pin to understand the state on DM35x, DM644x, DM646x, OMAPL13x platforms,

    You need to set the session bit in the controller.  In response to this the controller will do the required ID pin sense and appropriately generate either

    • a Drvvbus interrupt (if A end of cable is plugged in) or
    • initate a SRP on the USB bus (if vbus is not there) or
    • raise a reset interrupt (if VBUS is available and host issues the reset on the bus). 

    The later 2 cases signify Device mode while the 1st scenario signifies Host.

    Another interrupt you need to be aware of is the SRP interrupt that will be raised when a OTG cabapable device is connected and it requests for the VBUS to be turned on.  In this mode you again are in Host mode and would respond to the SRP interrupt by turning on the VBUS charge pump, afterwhich the regular process of enumerating the device proceeds.

    Pl. refer to the Linux USB driver for reference.  All these sequences are implemented and well tested at the least on DM35x platforms.

    regards

    swami

  • I just ran into one more interesting thing reguarding the USB interface.

    I added some ESD protection to the USB lines using a NUP4201 device from NXP.

    It contains a TVS diode for power line protection and fast diodes for transiant supression of the data lines. 

    I connected the power pin on the transient protection circuit to VBUS to hold the data lines within VBUS and ground (within a diode drop), but... because my OTG device switches VBUS on and off, when the VBUS is switched off I actually measure ~2.5V on my VBUS line due to the required bias of the ID line to 3.3V.

    I'm wondering if the ID pin on the DM357 is 5V tolerant so I could use VBUS to pull up the ID pin rather than 3.3V.  Otherwise, is there any reason I couldn't use a voltage divider from VBUS to ground connecting the middle net to the ID pin on the connector and the device if I create a voltage at the ID pin of ~3.3V referenced from VBUS.

    I guess my last option would be to add a second surge suppression circuit limiting the ID pin to 3.3V, this is probably the best option, but not something I'm really wanting to do.

     

    Anyhow, thanks for the feedback in advance.

     

  • Hi,swami

    when USB Device mode on DM644x,when should I set the DEVCTL.BDEVICE to initate a SRP on the USB bus,and when connect to Windows,how can make Windows find a new device?

     

    Thanks,

     

    tang

  • Tang,

    You should be setting the session bit to initiate SRP when connected to B end of cable.  When you connect to PC -host, PC-host would start of resetting DM644x device and you would not have to do anything in this case.

    regards

    swami

  • Swami

    Think you for your replay.But how can my program detect the connection of the B end of cable and DM644x?

     

    Thinks,

    Tang

  • Tang,

    Can you explain you exact usage context ?

    In the context of OTG one would not need to know the state of the cable end connected.  The controller along with the underlying driver takes care of this.  All the application has to do is to ask for a session.

    regards

    swami

  • Swami

    I want to use DM6446 as USB slave mode,I configured the linux USB driver as peripheral mode,after that, I connect DM6446 to PC-host with Windows XP,but the Windows did not find any new device.By the way, the USB ID pin is pulled up to 3.3V through 1.5K resistor.

    Could you please tell me what should I do to make Windows find a new device, 

    Think you very much,

    tang 

  • Tang,

    I think you need to leve the ID pin floating for Peripheral operation.  Can you try the use case after doing that?

    Pl. also refer to the EVM schematics for the way it has been accomplished.

    regards

    swami

  • Hi,

    I have a DM365 based customized hardware which has a hub chip with 4 ports. We are not able to detect USB pendrive or HDD on this. After readong number of posts on community, We suspect that USB is not working because USB_ID pin of the processor is left floating. It should be pulled down to ground by resistor.

    It seems hard to rework the board at this time. I am looking for a software work around for this if any. Please suggest..!!!

  • Hi,

    we also have a custom hardware with USB_ID pin floating :( Have you solved this with a software workaround?

    Regards

  • We had to put a 10k pull-up for device/otg mode on the ID line to make it work properly.

    Also, you might need to put a 1k pull-down on your USB_VBUS line to ensure it switches between device/host mode properly if using device and host functions/OTG.

     

    Seems like TI really should update their documentation here.

  • Hi,

    I am trying USB OTG support to dm365.

    Host was working when boot time plugged pen drive & at boot time not plugged pen drive after booting is not detected.
    ID pin configured below,
    USB ID=0 => Host
    USB ID=1 => Device

    root@edge-shelf:~# cat /proc/driver/musb_hdrc
    Status: MHDRC, Mode=Peripheral (Power=e0, DevCtl=99)
    OTG state: b_idle; inactive
    Options: cppi-dma, host, debug=0 [eps=5]
    Root port status: 00000000
    DaVinci: ctrl=00 stat=0 phy=21f0
            rndis=00000 auto=0000 intsrc=00000000 intmsk=01f71e1f
    CPPI: txcr=1 txsrc=0 txena=f; rxcr=1 rxsrc=0 rxena=f

    echo "F" > /proc/driver/musb_hdrc is not working to changed host mode. its always set Peripheral mode.

    BR
    Tejas

  • Hi,

    I am trying USB OTG support to dm365.

    Host was working when boot time pluged pendrive & at boot time not pluged pendrive after booting is not detected.
    ID pin configured below,
    USB ID=0 => Host
    USB ID=1 => Device

    root@edge-shelf:~# cat /proc/driver/musb_hdrc
    Status: MHDRC, Mode=Peripheral (Power=e0, DevCtl=99)
    OTG state: b_idle; inactive
    Options: cppi-dma, host, debug=0 [eps=5]
    Root port status: 00000000
    DaVinci: ctrl=00 stat=0 phy=21f0
    rndis=00000 auto=0000 intsrc=00000000 intmsk=01f71e1f
    CPPI: txcr=1 txsrc=0 txena=f; rxcr=1 rxsrc=0 rxena=f

    echo "F" > /proc/driver/musb_hdrc is not working to changed host mode. its always set Peripheral mode.

    BR
    Tejas