Part Number: AMIC110
Other Parts Discussed in Thread: AM3359, SYSBIOS
Tool/software: TI-RTOS
Hi all,
I am trying to get the Profinet examples to run. Here is the situation:
New install of Windows 10. There is NOTHING installed on this system except:
Code Composer Studio 8.3.0.00009
Processor SDK am335x-evm-05.01.00.11
PRU-ICSS-Profinet_Slave-01.00.03.04
I configure the profinet_slave_IRT_AMIC11x_arm project as described in the manual. I load the workspace in CCS. The compilation is successful. I create a target.ccxml (XDS110 Probe and AMIC110 profile, GEL file iceAMIC110.gel). I start a debug session on AMIC110 ICE EVM. It terminates with:
CortxA8: Unhandled ADP_Stopped exception 0x801AAD68
Next try: I switch to Build configuration: Debug. Compilation is successful. Debug session terminates with:
CortxA8: Unhandled ADP_Stopped exception 0x801B9568
Next try: I configure the profinet_slave_IRT_AM335x_arm project as described in the manual. I load the workspace in CCS. The compilation is successful. I create a target.ccxml (XDS100v2 Probe and ICE_AM3359 profile, GEL file TMDXICE3359.gel). I start a debug session on AM335x ICE v2. It terminates with:
CortxA8: Unhandled ADP_Stopped exception 0x801AB198
I did not try the debug build configuration...
There seems to be something wrong with either the example code or the documentation. I had similar behaviour on another workstation which had seen a lot of different installations of CCS's, PDK's etc. so I performed this clean install for troubleshooting. I need to get these examples running on EVMs to have a baseline for testing my custom design.
Regards,
Tom