Hi,
I would like to know the differences between TMS320C6748EZWTD4 and TMS320C6748EZWTA3.
As per datasheet, the difference between the two can be summarized as follows,
Parameter | TMS320C6748EZWTD4 | TMS320C6748EZWTA3 |
Operating junction temperature | - 40 to +90 °C | - 40 to +105 °C |
Speed grade | 456MHz | 375MHz |
Nominal CVDD voltage | 1.3V | 1.2V |
Power on hours (hours) | 100,000 | 75,000 |
Is there any other parameter (in terms of operational and reliability) which differs between these two part numbers?
Regards,
Archana Rao