This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OMAP3530/DM3730 SGX OpenGL Version Relation Ships

We are woking on OpenGL now, but we found that the SGX and OpenGL in Bsquare and Adeneo Embedded BSP is not the same. Bsquare BSP contains PowerVR-DDK-1.3.1_SDK-2.3.1_OMAP3530ES3.x_6.14.00.02, while Adeneo Embedded BSP contains PowerVR Rev121 and Rev125.  what is the  relationship between these bsp opengl?

Another quesiton: Adeneo Embedded BSP did not provide OpenGL Libs and Headers needed for developing applications, can we use libs and headers in Bsquare OpenGL packages?

 

Thanks & Best Regards,

 

Stephen Zhang