Part Number: PROCESSOR-SDK-AM335X
Other Parts Discussed in Thread: AM3359
Tool/software: Linux
We've a custom board based on AM335x-EVM-Starter Kit.
SDK we're using is ti-processor-sdk-linux-am335x-evm-05.00.00.15.
In the above schematic, the following 3 lines are connected to the FPGA.
1. UART1_CTSn,
2. UART1_RTSn &
3. GPMC_BEn0_CLE
Our requirement is to prove the clock rate as 10 MHz on all the above 3 lines.
1. We want to send some buffer from processor (ex:- an array of 1024 bytes) to FPGA and capture the data. How to do it?
2. If any thing to be set in the kernel, where and all I should modify?
Please find below my dts file & the program that I am using to send data to FPGA, Please suggest me changes required, if any.
DTS:
gpio1_pins:gpio1_pins{
pinctrl-single,pins = <
AM33XX_IOPAD(0x978, PIN_OUTPUT | MUX_MODE7) /*UART1_CTSn.GPIO0_12*/
AM33XX_IOPAD(0x97c, PIN_OUTPUT | MUX_MODE7) /*UART1_RTSn.GPIO0_13*/
AM33XX_IOPAD(0x89c, PIN_OUTPUT | MUX_MODE7) /*GPMC_BEn0_CLE.GPIO2_5*/
>;
};
&gpio1 {
pinctrl-names = "default";
pinctrl-0 = <&gpio1_pins>;
status = "okay";
};
Program to send data to FPGA:
#include <stdlib.h>
#include <stdio.h>
#include <unistd.h>
#include <stdio.h>
#include <stdlib.h>
#include <string.h>
#include <fcntl.h>
#include <unistd.h>
#include <sys/select.h>
#include <sys/stat.h>
#include <time.h>
#include <getopt.h>
//#include "gpiolib.h"
int gpio_export(int gpio)
{
int efd;
char buf[50];
int gpiofd, ret;
/* Quick test if it has already been exported */
sprintf(buf, "/sys/class/gpio/gpio%d/value", gpio);
efd = open(buf, O_WRONLY);
if(efd != -1) {
close(efd);
return 0;
}
efd = open("/sys/class/gpio/export", O_WRONLY);
if(efd != -1) {
sprintf(buf, "%d", gpio);
ret = write(efd, buf, strlen(buf));
if(ret < 0) {
perror("Export failed");
return -2;
}
close(efd);
} else {
// If we can't open the export file, we probably
// dont have any gpio permissions
return -1;
}
return 0;
}
void gpio_unexport(int gpio)
{
int gpiofd, ret;
char buf[50];
gpiofd = open("/sys/class/gpio/unexport", O_WRONLY);
sprintf(buf, "%d", gpio);
ret = write(gpiofd, buf, strlen(buf));
close(gpiofd);
}
int gpio_read(int gpio)
{
char in[3] = {0, 0, 0};
char buf[50];
int nread, gpiofd;
sprintf(buf, "/sys/class/gpio/gpio%d/value", gpio);
gpiofd = open(buf, O_RDWR);
if(gpiofd < 0) {
fprintf(stderr, "Failed to open gpio %d value\n", gpio);
perror("gpio failed");
}
do {
nread = read(gpiofd, in, 1);
} while (nread == 0);
if(nread == -1){
perror("GPIO Read failed");
return -1;
}
close(gpiofd);
return atoi(in);
}
int gpio_write(int gpio, unsigned char val)
{
char buf[50];
int nread, ret, gpiofd;
sprintf(buf, "/sys/class/gpio/gpio%d/value", gpio);
gpiofd = open(buf, O_RDWR);
if(gpiofd > 0) {
snprintf(buf, 2, "%d", val);
ret = write(gpiofd, buf, 2);
if(ret < 0) {
perror("failed to set gpio");
return 1;
}
close(gpiofd);
if(ret == 2) return 0;
}
return 1;
}
int gpio_direction(int gpio, int dir)
{
int ret = 0;
char buf[50];
sprintf(buf, "/sys/class/gpio/gpio%d/direction", gpio);
int gpiofd = open(buf, O_WRONLY);
if(gpiofd < 0) {
perror("Couldn't open IRQ file");
ret = -1;
}
if(dir == 2 && gpiofd){
if (3 != write(gpiofd, "high", 3)) {
perror("Couldn't set GPIO direction to out");
ret = -2;
}
}
if(dir == 1 && gpiofd){
if (3 != write(gpiofd, "out", 3)) {
perror("Couldn't set GPIO direction to out");
ret = -3;
}
}
else if(gpiofd) {
if(2 != write(gpiofd, "in", 2)) {
perror("Couldn't set GPIO directio to in");
ret= -4;
}
}
close(gpiofd);
return ret;
}
int main(int argc, char **argv) {
int gpio_pin1 = 12,gpio_pin2=13,gpio_pin3=69,i;
struct timespec tim, tim2;
tim.tv_sec = 0;
tim.tv_nsec = 50;
gpio_export(gpio_pin1);
gpio_direction(gpio_pin1, 1);
gpio_export(gpio_pin2);
gpio_direction(gpio_pin2, 1);
gpio_export(gpio_pin3);
gpio_direction(gpio_pin3, 1);
unsigned char value=12;
while(1)
{
gpio_write(gpio_pin1,value);
gpio_write(gpio_pin2,value);
gpio_write(gpio_pin3,value);
usleep(10);
//nanosleep(&tim, NULL);
//value = value ? 0:1;
//printf("val: %d\n",value);
}
gpio_unexport(gpio_pin1);
gpio_unexport(gpio_pin2);
gpio_unexport(gpio_pin3);
return 0;
}
Thanks & Regards
Vamsi