Part Number: BEAGLEBK
Hello all,
I am currently working on the following project 0
dev.ti.com/.../154-stack_03_linux_project_0.html
I am working on task 3 in the above link , titled Task 3: Install the TI-15.4 Stack Linux Gateway SDK
I installed this file by following the link , ti154stack_linux_x64_2_08_00_04.run
and through the Linux terminal ( I am using Linux Mint 19) I navigated to the folder where the above file is installed , and I put the following commands in the terminal as stated per the instructions:
neil@neil-LIFEBOOK-AH531:~/Downloads$ +x ti15.4stack_linux_x64_2_08_00_04.run$./ti15.4stack_linux_x64_2_08_00_04.run
+x: command not found
neil@neil-LIFEBOOK-AH531:~/Downloads$ ti15.4stack_linux_x64_2_08_00_04.run$./ti15.4stack_linux_x64_2_08_00_04.run
bash: ti15.4stack_linux_x64_2_08_00_04.run$./ti15.4stack_linux_x64_2_08_00_04.run: No such file or directory
Any help would be appreciated. Regards.
Neil Mustafa.