This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RTOS / TDA2EG-17: AVM Solution on TDA serial

Part Number: TDA2EG-17

Tool/software: TI-RTOS

Hi TI expert

I have some questions.

Q1. Could  i TDA2EG-17 receive  4ch 1280P or 1080P @ 30 Yuv422 (8bit) on VIP ? if can't , How about TDA2-EG or TDA2P ?

Q2.Could i use D0~D7 output 1080P @30fps Yuv422 BT.601/BT.656 on the TDA2EG-17 LCD3 Port ? I implemented D0~D7 output  720P @ 30fps Yuv422 BT.601 on the TDA2EG-17 LCD 3 port.

Q3.From above questions,should I use 913 and 914 to transfer data or 933 and 934 to transfer?

  • 1. A single VIP port can capture 8-bit 1080p @ 30 FPS or 720p @ 30FPS. Kindly refer to the device/part manual to see if all the 4 VIP pins can be used. Also as long as the input to the VIP is less than 165 MHz, then it can capture 1920x1280p as well.
    2. 1080p30 8-bit is not validated in DSS driver
    3. Kindly refer to serializer manual to check if it supports the required pixel clock