This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM365 EVM does not boot

Hi,

I modified my DM365 EVM board a little (mainly related to the CPLD) and found it does not boot. Then I change back to original. It still does not boot. - There is nothing showing on hyper terminal from serial port. That means the u-boot on NAND flash does not start.

What can I do now to verify whether or not the DM365 processor or the NAND flash damaged? Is it possible that some of the pins of DM365 processor or the NAND flash damaged? The overall current is about 760mA@ +5V input. Thanks.

 

Jonathan