Hi,
to make some PRU performance measurements, I would like to use the Cycle Count.
The TRM describe the physical address of PRU_ICSSG_0_PR1_PDSP0_IRAM to 0xB02200. The Cycle Count Register at 0xB0220C. However the memory at these address does not change when PRU is running.
However, after some time I disovered that at address 0xB02200C some data is placed, which could be the Cycle Count Register for ICSSG0_PRU0.
Can you confirm this?
If yes, why is there a 0 missing in the TRM?
Best regards,
Thomas