I tested DM355 IPIPE block using MT9T001 CMOS Sensor.
The following information is relevant parameters.
. CMOS Frame Rate : about 30 fps
. CMOS output : 1024 * 768 ( convert 2048*1536 format to it by 2x bining)
. CCDC Input format: 1024 * 768
. IPIPE Output : VGA (640*480) ; by IPIPE resizer
But.. because VD(10 pixel), HD(8 pixel), Black looks in the left side and bottom of the below captured image.
What is the problem ?