I am using APPRO's IPNC with software load 0.7 and am seeing some video issues as seen below.
The one above is in single stream H.264 D1 mode with H3A turned on. This is continuous, with the lines and colours only shifting slightly.
This one is in single stream H.264, 720P resolution. It looks like the video row data is being compressed for some reason and then black shown on the remainder of the line. This happens on both the TV out and the RTSP stream, however it only happens occasionally.
I have added some debug prints, but haven't changed any settings. The system is running off NFS root.
Any ideas on what might cause these or where we should look for the problem/solution? Could this be caused by hardware issues?
Thanks,
Quinn.