This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM5728: user application for storing data to emmc

Part Number: AM5728


Tool/software: Linux

hai,

i am working on am5728 . I am working with temperature sensors connected to it through i2c. My application is working and saves the log of data into a text file when working on SD card but i want to use emmc and use it for storing the application and also save log text file in it.

i have also made the emmc partitions but i want to know to write an user application for storing text file or any file that is to be stored on emmc.

can anyone help with issue.

Thanks & Regards,

venkat R.