This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

dmai bug? Can't reopen capture device..

Dear all,

       My board is dm6446-evm. dmai version is dmai_1_10_00_06, lsp is lsp-120.

      I  just do a simple test to reopen the capture device, I add some code at the end of the loop of the video_loopback_copy example:
        index++;
        if (index == 100) {
                printf("change once!\n");
                Capture_delete(hCapture);
                sleep(1);
                hCapture = Capture_create(NULL, &cAttrs);
                index = 0;
        }

    I found that the first "Capture_delete"  didn't switch to the kernel release function "vpfe_release" unless the second Capture_create is called!

     Same  operation in dvsdk/demos will be OK.

    This is very strange, please kindly test for this bug. Attachment is my source code.

    Thanks you!

   Wei Jiang