Part Number: AM5728
Tool/software: TI-RTOS
hello.
The board I'm using is the AM572x Evaluation Module (TMDSEVM572X), and the downloaded RTOS SDK version is 5.02.
I have a question about DSS scaler.
The manual states that all input formats are supported. However, the VPE driver description states that only YUV format input is supported.
Did I get it right?
So the question is, should I use the only YUV input format to implement the scaler function using the VPE driver?
And if not, I wonder if there is a DSS scaler example that uses RGB as input format.
please answer me.
Thank you.