Hi,
I am working on a couple of DM365 EVMs and I need to restore ubl and u-boot on one of them. I am using DM644x serial flasher 1.50. After setting up the UART boot mode before flashing the board, I attempted to flash the board -unsuccessfully- with the binary files included in the PSP. I do not get the usual BOOTME prompt in a Minicom terminal but rather a version of it with some non-printable symbols that I suppose prevent the flasher from taking control. I tested the two boards and both of them exhibit the same behaviour. I also tested the configuration of my terminal (Minicom) in case some setting could be wrong against a DM355 EVM, but everything normal.
Has anyone experienced something like this? Any ideas?
Regards,
Santiago.