This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Steps to flash uboot and ubl to a 256K Block Size NAND Flash chip (MT29F16G08DAA)



Hi

I have been going through the steps of serial programming from the website for the TI Serial utility as well as the 7 steps posted on this forum.  The Serial sfh_DM35x.exe says each time that it has been programmed successfully, but I dont think I have the start locations correctly set up.  I checked the original part that is currently on the DM355 Board which is MT29F16G08FAA, and it has a block size of 128K, and so I am wondering about what are the starting locations in order for me to flash the NAND chip that I have. 

Essentially what I would like to know is what values should I be putting in for UBLStartAddr AppLoadAddr and AppStartAddr so that I can get the NAND to boot.

Currently after all those steps it just sits there, and I get no promt or anything once I cycle power and switch SW7 to boot from NAND.