This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM5728: KSZ9031 issue with PRU Ethernet

Part Number: AM5728
Other Parts Discussed in Thread: TLK105

Tool/software: Linux

Hi,

We have designed the custom board for four Ethernet requirements. Two dedicated RGMII ethernet ports for 1Gbps have been used and other two through PRU have been used to cater our requirements.

In our design we have used same PHY KSZ9031 for all the four ethernets.

Now, when we power ON only two RGMII ethernets have been accessed for communication, other two PRU ethernets are detected but there is no communication.

please clarify  whether PHY KSZ9031 is compatible for PRU ethernet or not, and suggest what should be done or which PHY is suitable for working with PRU ethernet.

BR

satya