This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/RFSDK: K2l RFSDK JESD initialization Issue in 4 lane configuration

Part Number: RFSDK


Tool/software: Linux

Hi,

We are working on K2l with rfsdk version 2.0.6.0  with our own custom RF card which is JESD compatible.

We are using 4 lane (2x2-4xLTE20-SC-JESD1-HD) configuration file.RF card is initialized and JESD setup is complete.Both framer and De-framer Jesd status is fine on RF card.

On K2l JESD side sync state of all the lanes is  2 which indicates successful initialization.

Code state for lane 0 and 2 is  2.

Code state for lane 1 and 3 is  0.These two lanes are not  initialized.

Out of four lanes which 2 lanes are used for rx framer and observation path?

Do we need any changes on RFSDK to initialize all the lanes ?.

Suggestions would be helpful.

Thanks,

sandeep