Part Number: TMS320C6711D
We are using a TMS320C6711DZDP200 in our design..
Our CLKIN has a 150MHz clock input...After continuous operation for an hour or two the System Locks up. We have isolated it down to the DSP and possibly the 150MHz clock input. We do not have a WDT in the design..Our ECLKIN signal is 100MHz.. our ECLKOUT is 100MHz... What I cannot tell is if it is the DSP how can I prove it.. My series terminated resistor is 240 ohms.. My 150MHz is coming from an Altera MAX 10 FPGA.. The 240 is high... The Lockups only occur on a few of our boards.. Any suggestions?