Part Number: AM5718
Other Parts Discussed in Thread: TPS65916
Tool/software: Linux
Hi,
We developed a custom board based on AM5718 + TPS65916. The system clock used is 24MHz. The DS says the clocks supported are 19.2, 20 or 27 Only. In that case 24MHz can not be used ?
If it can be used where can I change the System clock in u-boot so that the right clocks are generated for other peripherals.
Best Regards, Prasad