This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/TCI6630K2L: RFSDK JESD initialization issue

Part Number: TCI6630K2L


Tool/software: Linux

Hi,

We are working on K2l with rfsdk version 2.0.6.0  with our own custom RF card which is JESD compatible.

We are using 4 lane (2x2-4xLTE20-SC-JESD1-HD) configuration file.RF card is initialized and JESD setup is complete.Both framer and De-framer Jesd status is fine on RF card.

On K2l JESD side sync state of all the lanes is  2 which indicates successful initialization.

If we change crossbar lane selection on the RF  code state changes.

If the  crossbar  selection on rf card is  E4 then  Code state for lanes 0,2 is  2 and  lane 1,3 is  0.

If the  crossbar  selection on rf card is changed to D8 then  Code state for lanes 1,2 is  2 and  lane 0,3 is  0.

For any cross bar selection only 2 lanes are initialized properly.

Do we have to change .tgt config file to initialize all the  lanes?

Out of four lanes which 2 lanes are used for Rx framer and observation path ?

Suggestions would be helpful.

Thanks,

sandeep