This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/TDA2PXEVM: Is DVFS supported for GFX?

Part Number: TDA2PXEVM

Tool/software: Linux

hi,

I'm working on TDA2PX processor with PROCESSOR_SDK_VISION_03_04_00_00, and want to konw whether DVFS is supported for SGX module?

the GPU performance util pvrscope shows that SGX is always kept at fixed frequency at 532MHz no matter how heavy the 3D render loading is.

prvscope logs:

| | | | | |
| VDD_GPU / VDD_CORE2 | 78C / 172F | NA | | HIGH |
| GPU | | | 532 MHz | |
| | | | | |

If DVFS for SGC is supported, could you kindly explain how to enable?

Thanks!

Brs

--Yanchang