Greetings:
I got my DM365EVM today and connect the DVEVM as the instruction, but I couldn't see the video output on my display screen.
Then I connect the UART and found some problems about capture initializing failure. The information is as below:
VFS: Mounted root (yaffs2 filesystem).
Freeing init memory: 168K
INIT: Entering runlevel: 3
Starting internet superserver: inetd.
Starting audio loopback demo
Starting video loopback demo
ths7353_setvalue -start
main : Enter
vpbe_UE_1 : Enter
initializing capture device
ths7353_setvalue -end
ths7353_setvalue -start
setting data format
Detecting if driver supports COMPONENT
input.name = RAW
input.name = RAW-1
input.name = COMPOSITE
input.name = SVIDEO
input.name = COMPONENT
ths7353_setvalue -end
querystd, erorxxx, val = 1, val1 = 1
error: InitDevice:ioctl:VIDIOC_G_INPUT
Error in setting capture format
Failed to intialize capture
main : Leave
What will the problem probably be? Thanks for any advice or hint.
Best regards;