This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM5718: Arago/Yocto wpa-supplicant version question

Part Number: AM5718


Tool/software: Linux

Hello,

I'm trying to build a custom image based on the arago distribution corresponding to SDK 05.02.00.10.

My project will use an USB wifi dongle and I need to include the wpa-supplicant package.

However, if I put IMAGE_INSTALL_append = " wpa-supplicant" in my image recipe the build process pulls in wpa-supplicant-wl18xx from the meta-arago layer, which seems to be a custom version for the TI WL18XX modules.

How can override this behavior and use the recipe from oe-core/meta layer? I tried setting PREFERRED_VERSION_wpa-supplicant="2.6" but did not make any difference. The only thing that seems to work is removing the wpa-supplicant-wl18xx.bb recipe from meta-arago, but I'm thinking there has to be a better way.

Please advise,

--Tavi