This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM357 UBL source code can not run on EVM board

I am using DM357 EVM board,when I compile UBL code (DM357_FlashAndBootUtils_1_50),but it can not run,

when I config board in UART boot mode ,it print BOOTME from uart port

when I config as other boot mode,it do nothing,and don't print any thing from UART port

I am using CCS3.3,560PLUS

but the UBL bin file from TI can run on the board.

does any body has compiled the  UBL code(DM357_FlashAndBootUtils_1_50)?

Thanks for you help!

  • I am using DM357 EVM board too, I can't  write UBL, UBOOT, UIMAGE with NANDwriter.out (from  /home/<useracct>/dvsdk_#_##/PSP_#_#_#_#/bin/dm357), when i load and run it,nothing display.  so I can't burn these file to NAND.  and I have't  source code of NANDwriter  ,have't source of UBL. where you get these source code? Can you give me? I test the same things. We can help eachother. my msn:  neusoft_david@hotmail.com.