This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Triple resizing in IPNC 2.0 dm368 possible ?

I tested the triple resizing and encoding in ipnc 2.0 dm368. It is offering only 17 fps.

If I change the config->resizerClkdivN = 40 , it does triple streaming . But after some time it hangs.

Have anybody tried this on Dm368?  It works for dm365.

 

 

  • Hi,

    Which triple streaming usecase are you trying? Can you provide some details about the mode, so that we can figure out the issue? We need resolution details in this usecase

    Regards,

    Anshuman

  • in 720P mode with SONY IMX sensor

  • I will have to check with the team on how they expect the performance on IMX sensor IPNC. Which is the sensor IMX035 or IMX036?

    Can you share the profile log on the terminal so that i can help further?

     

    Regards,

    Anshuman

  • It is IMX036. The logs are given below.

    It is not giving 30fps in ddr resizing mode as you see it in the profiler. 

     

     

    Starting kernel ...    

                                                                                                                                         
                                                                                                                                                                
    Linux version 2.6.18_pro500-davinci_IPNC_DM368_2.0.0 (wenchi@dino.linux) (gcc version 4.2.0 (MontaVista 4.2.0-16.0.32.0801914 2008-08-30)) #1 PREEMPT Thu Ju0
    CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177                                                                                               
    Machine: DaVinci DM368 IPNC                                                                                                                                 
    Memory policy: ECC disabled, Data cache writeback                                                                                                           
    DaVinci DM0365 variant 0x8                                                                                                                                  
    PLL0: fixedrate: 24000000, commonrate: 170000000, vpssrate: 340000000                                                                                       
    PLL0: vencrate_sd: 75555555, ddrrate: 340000000 mmcsdrate: 48571428                                                                                         
    PLL1: armrate: 432000000, voicerate: 20571428, vencrate_hd: 27000000                                                                                        
    CPU0: D VIVT write-back cache                                                                                                                               
    CPU0: I cache: 16384 bytes, associativity 4, 32 byte lines, 128 sets                                                                                        
    CPU0: D cache: 8192 bytes, associativity 4, 32 byte lines, 64 sets                                                                                          
    Built 1 zonelists.  Total pages: 12800                                                                                                                      
    Kernel command line: mem=50M console=ttyS1,115200n8 root=/dev/ram0 rw initrd=0x82000000,16M eth=00:0C:0C:A0:04:B5                                           
    PID hash table entries: 256 (order: 8, 1024 bytes)                                                                                                          
    Clock event device timer0_0 configured with caps set: 07                                                                                                    
    Console: colour dummy device 80x30                                                                                                                          
    Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)                                                                                               
    Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)                                                                                                
    Memory: 50MB = 50MB total                                                                                                                                   
    Memory: 30208KB available (3117K code, 647K data, 176K init)                                                                                                
    Security Framework v1.0.0 initialized                                                                                                                       
    Capability LSM initialized                                                                                                                                  
    Mount-cache hash table entries: 512                                                                                                                         
    CPU: Testing write buffer coherency: ok                                                                                                                     
    checking if image is initramfs...it isn't (bad gzip magic numbers); looks like an initrd                                                                    
    Freeing initrd memory: 16384K                                                                                                                               
    NET: Registered protocol family 16                                                                                                                          
    DaVinci: 104 gpio irqs                                                                                                                                      
    MUX: initialized GPIO20                                                                                                                                     
    MUX: initialized I2C_SCL                                                                                                                                    
    Generic PHY: Registered new driver                                                                                                                          
    ch0 default output "COMPOSITE", mode "NTSC"                                                                                                                 
    VPBE Encoder Initialized                                                                                                                                    
    SCSI subsystem initialized                                                                                                                                  
    NET: Registered protocol family 2                                                                                                                           
    IP route cache hash table entries: 512 (order: -1, 2048 bytes)                                                                                              
    TCP established hash table entries: 2048 (order: 1, 8192 bytes)                                                                                             
    TCP bind hash table entries: 1024 (order: 0, 4096 bytes)                                                                                                    
    TCP: Hash tables configured (established 2048 bind 1024)                                                                                                    
    TCP reno registered                                                                                                                                         
                                                                                                                                                                
     ***davinci_spi_board_init()!<6>                                                                                                                            
     ***davinci_spi_board_init_End(0)!<5>VFS: Disk quotas dquot_6.5.1                                                                                           
    Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)                                                                                                  
    squashfs: version 3.1 (2006/08/19) Phillip Lougher                                                                                                          
    JFFS2 version 2.2. (NAND) (C) 2001-2006 Red Hat, Inc.                                                                                                       
    yaffs Jul 29 2010 14:32:38 Installing.                                                                                                                      
    SGI XFS with no debug enabled                                                                                                                               
    Initializing Cryptographic API                                                                                                                              
    io scheduler noop registered                                                                                                                                
    io scheduler anticipatory registered (default)                                                                                                              
    LTT : ltt-facilities init                                                                                                                                   
    LTT : ltt-facility-core init in kernel                                                                                                                      
    DAVINCI-WDT: DaVinci Watchdog Timer: heartbeat 60 sec                                                                                                       
    Serial: 8250/16550 driver $Revision: 1.90 $ 2 ports, IRQ sharing disabled                                                                                   
    serial8250.0: ttyS0 at MMIO map 0x1c20000 mem 0xfbc20000 (irq = 40) is a 16550A                                                                             
    serial8250.0: ttyS1 at MMIO map 0x1d06000 mem 0xfbd06000 (irq = 41) is a 16550A                                                                             
    RAMDISK driver initialized: 1 RAM disks of 32768K size 1024 blocksize                                                                                       
    Linux video capture interface: v2.00                                                                                                                        
    Trying to register davinci display video device.                                                                                                            
    layer=c2e74a00,layer->video_dev=c2e74b60                                                                                                                    
    Trying to register davinci display video device.                                                                                                            
    layer=c2e74800,layer->video_dev=c2e74960                                                                                                                    
    davinci_init:DaVinci V4L2 Display Driver V1.0 loaded                                                                                                        
    i2c /dev entries driver                                                                                                                                     
    nand_davinci nand_davinci.0: Using 4-bit hardware ECC                                                                                                       
    NAND device: Manufacturer ID: 0xec, Chip ID: 0xf1 (Samsung NAND 128MiB 3,3V 8-bit)                                                                          
    Creating 7 MTD partitions on "nand_davinci.0":                                                                                                              
    0x00000000-0x00300000 : "bootloader"                                                                                                                        
    0x00300000-0x00500000 : "params"                                                                                                                            
    0x00500000-0x00700000 : "kernel"                                                                                                                            
    0x00700000-0x02700000 : "filesystem"                                                                                                                        
    0x02700000-0x02900000 : "data1"                                                                                                                             
    0x02900000-0x02d00000 : "Calibration"                                                                                                                       
    0x02d00000-0x08000000 : "data2"                                                                                                                             
    nand_davinci nand_davinci.0: hardware revision: 2.3                                                                                                         
    MUX: initialized SPI0_SCLK                                                                                                                                  
    MUX: initialized SPI0_SDO)                                                                                                                                  
    dm_spi.0: davinci SPI Controller driver at 0xc3866000 (irq = 42) use_dma=0                                                                                  
    rtc_davinci_dm365 rtc_davinci_dm365.0: rtc intf: proc                                                                                                       
    rtc_davinci_dm365 rtc_davinci_dm365.0: rtc intf: dev (254:0)                                                                                                
    rtc_davinci_dm365 rtc_davinci_dm365.0: rtc core: registered rtc_davinci_dm365 as rtc0                                                                       
    Advanced Linux Sound Architecture Driver Version 1.0.12rc1 (Thu Jun 22 13:55:50 2006 UTC).                                                                  
    ASoC version 0.13.1                                                                                                                                         
    CQ0093 Voice Codec 0.1                                                                                                                                      
    asoc: cq93vc <-> davinci-vcif mapping ok                                                                                                                    
    ALSA device list:                                                                                                                                           
      #0: On-chip voice codec (cq93vc)                                                                                                                          
    IPv4 over IPv4 tunneling driver                                                                                                                             
    TCP bic registered                                                                                                                                          
    NET: Registered protocol family 1                                                                                                                           
    NET: Registered protocol family 17                                                                                                                          
    rtc_davinci_dm365 rtc_davinci_dm365.0: setting the system clock to 2010-12-03 03:38:08 (1291347488)                                                         
    Time: timer0_1 clocksource has been installed.                                                                                                              
    Clock event device timer0_0 configured with caps set: 08                                                                                                    
    Switched to high resolution mode on CPU 0                                                                                                                   
    IP-Config: No network devices available.                                                                                                                    
    RAMDISK: cramfs filesystem found at block 0                                                                                                                 
    RAMDISK: Loading 11896KiB [1 disk] into ram disk... done.                                                                                                   
    VFS: Mounted root (cramfs filesystem) readonly.                                                                                                             
    Freeing init memory: 176K                                                                                                                                   
    INIT: version 2.86 booting                                                                                                                                  
    0                                                                                                                                                           
    mkdir: Cannot create directory `/dev/.test': Read-only file system                                                                                          
    Starting the hotplug events dispatcher: udevd.                                                                                                              
    Synthesizing the initial hotplug events...done.                                                                                                             
    Waiting for /dev to be fully populated...done.                                                                                                              
    0                                                                                                                                                           
    CSL: Module install successful, device major num = 253                                                                                                      
    CSL: Module version 0.10.00, built on Jul 14 2010 17:49:32                                                                                                  
    I2C: Module install successful, device major num = 252                                                                                                      
    DMA: Module install successful, device major num = 251                                                                                                      
    DRV: Module install successful                                                                                                                              
    DRV: Module built on Jul 14 2010 17:49:33                                                                                                                   
    DRV: EDMACC.QUEPRI  = 00000777                                                                                                                              
    DRV: SYSTEM.MSTPRI0 = 00550011                                                                                                                              
    DRV: SYSTEM.MSTPRI1 = 00000444                                                                                                                              
    DRV: ISP.BCR        = 00000002                                                                                                                              
    DRV: SYSTEM.MISC = 00000311                                                                                                                                 
    CMEMK module: built on Jul 14 2010 at 17:48:57                                                                                                              
      Reference Linux version 2.6.18                                                                                                                            
      File /home/wenchi/Templates/DM365_IMX035/dvsdk_2_10_01_18_368/linuxutils_2_24_03/packages/ti/sdo/linuxutils/cmem/src/module/cmemk.c                       
    allocated heap buffer 0xc4000000 of size 0x4e00000                                                                                                          
    CMEM Range Overlaps Kernel Physical - allowing overlap                                                                                                      
    CMEM phys_start (0x1000) overlaps kernel (0x80000000 -> 0x83200000)                                                                                         
    cmemk initialized                                                                                                                                           
    EDMAK module: built on Jul 14 2010 at 17:49:01                                                                                                              
      Reference Linux version 2.6.18                                                                                                                            
      File /home/wenchi/Templates/DM365_IMX035/dvsdk_2_10_01_18_368/linuxutils_2_24_03/packages/ti/sdo/linuxutils/edma/src/module/edmak.c                       
    IRQK module: built on Jul 14 2010 at 17:49:02                                                                                                               
      Reference Linux version 2.6.18                                                                                                                            
      File /home/wenchi/Templates/DM365_IMX035/dvsdk_2_10_01_18_368/linuxutils_2_24_03/packages/ti/sdo/linuxutils/irq/src/module/irqk.c                         
    irqk initialized                                                                                                                                            
    Creat queue id:0                                                                                                                                            
    queue id:0                                                                                                                                                  
    Creat queue id:32769                                                                                                                                        
    queue id:32769                                                                                                                                              
    Creat queue id:65538                                                                                                                                        
    queue id:65538                                                                                                                                              
    IPNC_DM368_2.0.0 (wenchi@dino.linux) (gcc version 4.2.0 (MontaV                                                                                             
    queue id:65538                                                                                                                                              
    queue id:32769                                                                                                                                              
                                                                                                                                                                
     DEMOCFG Value: 0                                                                                                                                           
                                                                                                                                                                
    nVideocodecmode = 0                                                                                                                                         
    nVideocodecres = 0                                                                                                                                          
    ./av_server.out FD OSD AEWB APPRO2A 720P H264 4000000 CBR MENUOFF &                                                                                         
    Check_device_version : DEVICE VER = 0 !!                                                                                                                    
    Starting mounting local filesystems:                                                                                                                        
     AVSERVER UI: Initializing.                                                                                                                                 
                                                                                                                                                                
    DRV_SyncRst: module = 47, domain = 0, state = 0                                                                                                             
                                                                                                                                                                
    DRV_SyncRst: module = 47, domain = 0, state = 3                                                                                                             
    mount none on /dev/shm type tmpfs (rw,size=5M)                                                                                                              
    none on /var/run type tmpfs (rw)                                                                                                                            
    none on /tmp type tmpfs (rw,sync)                                                                                                                           
                                                                                                                                                                
     CLK Hz,                                                                                                                                                    
     ARM   Hz =  432000000                                                                                                                                      
     DDR   Hz =  340000000                                                                                                                                      
     VPSS  Hz =  340000000                                                                                                                                      
     IMCOP Hz =  340000000                                                                                                                                      
                                                                                                                                                                
     DRV LDC: GetConfig 0004 0x0                                                                                                                                
    Setting up networking ...rm: unable to remove `/etc/network/run': Read-only file system                                                                     
    numid=2,iface=MIXER,name='Mono DAC Playback Volume'                                                                                                         
      ; type=INTEGER,access=rw---,values=1,min=0,max=63,step=0                                                                                                  
      : values=32                                                                                                                                               
    ApproDrvInit: 7                                                                                                                                             
    Creat queue id:98307                                                                                                                                        
    queue id:98307                                                                                                                                              
    Starting hotplug subsystem:                                                                                                                                 
     AVSERVER UI: Starting in mode 1                                                                                                                            
    ############OPEN###########                                                                                                                                 
     Sensor Mode Info,                                                                                                                                          
     Width      = 2024                                                                                                                                          
     Height     = 1140                                                                                                                                          
     fps        =   24                                                                                                                                          
     Bin Enable =    1                                                                                                                                          
                                                                                                                                                                
     Sensor Frame Timing Info,                                                                                                                                  
     fps                  = 24                                                                                                                                  
     t_frame (ns)         = 41666668.000000                                                                                                                     
     t_row   (ns)         = 30458.333984                                                                                                                        
     t_pclk  (ns)         = 10.416667                                                                                                                           
     W                    = 2024                                                                                                                                
     H                    = 1140                                                                                                                                
     SW                   = 1406                                                                                                                                
     SD                   = 0                                                                                                                                   
     HB                   = 450                                                                                                                                 
     VB                   = 227                                                                                                                                 
     HBmin                = 450                                                                                                                                 
     VBmin                = 9                                                                                                                                   
     f_pclk               = 96000000                                                                                                                            
     shutterOverhead (ns) = 4437.500000                                                                                                                         
     col_size             = 2024                                                                                                                                
     row_size             = 1140                                                                                                                                
     col_bin              = 0                                                                                                                                   
     row_bin              = 0                                                                                                                                   
     col_start            = 88                                                                                                                                  
     row_start            = 276                                                                                                                                 
     pll_M                = 16                                                                                                                                  
     pll_N                = 1                                                                                                                                   
     pll_DIV              = 1                                                                                                                                   
                                                                                                                                                                
    ############reset###########                                                                                                                                
       pci                                                                                                                                                      
       pci      [success]                                                                                                                                       
    ############SPI OPEN###########                                                                                                                             
    spi mode: 16                                                                                                                                                
    bits per word: 8                                                                                                                                            
    max speed: 12000000 Hz (12000 KHz)                                                                                                                          
    ############SET REG###########                                                                                                                              
    ############OPEN END###########                                                                                                                             
    ================> 1023, 0, 1607                                                                                                                             
    APPRO Setting Applied                                                                                                                                       
                                                                                                                                                                
     Default Icon TI Logo                                                                                                                                       
                                                                                                                                                                
     Default Icon TI Logo                                                                                                                                       
                                                                                                                                                                
     Default Icon TI Logo                                                                                                                                       
                                                                                                                                                                
     DM365MM Init SuccessfulRate Control Type: IVIDEO_LOW_DELAY STREAM: Ext 0: 0x0                                                                              
     STREAM: Ext 1: 0x0                                                                                                                                         
    queue id:98307                                                                                                                                              
    FF: FF open                                                                                                                                                 
                                                                                                                                                                
     FR : 0 users registered DavinciDisplay DavinciDisplay.1: Before finishing with S_FMT:                                                                      
    layer.pix_fmt.bytesperline = 640,                                                                                                                           
     layer.pix_fmt.width = 640,                                                                                                                                 
     layer.pix_fmt.height = 480,                                                                                                                                
     layer.pix_fmt.sizeimage =460800                                                                                                                            
    from exsiting faDavinciDisplay DavinciDisplay.1: pixfmt->width = 640,                                                                                       
     layer->layer_info.config.line_length= 640                                                                                                                  
    ce album                                                                                                                                                    
    FF: FF open done.                                                                                                                                           
    IPNC_DM368_2.0.0 (wenchi@dino.linux) (gcc version 4.2.0 (MontaV                                                                                             
     IPNC AUTO_IRIS = 0 (0:Manual,1:Auto)#####################                                                                                                  
    APPRO 2A Created                                                                                                                                            
    XXXXX IAE_CMD_SET_CONFIG XXXXX                                                                                                                              
       usb                                                                                                                                                      
                                                                                                                                                                
     222 Aew_Cal_LoadParam: dfc check sum success                                                                                                               
     (nand offset: 0x00500010, size: 0x0000181c, checksum: 0x00021e46)                                                                                          
    ################DFC ret=0##################                                                                                                                 
    DFC number:255                                                                                                                                              
    EE SETUP SHIFT VALUE: 3                                                                                                                                     
    GBCE in EVAL MODE                                                                                                                                           
    AUDIO_GetSampleRate = 8000                                                                                                                                  
    AUDIO : period size = 1000 frames dir = 0                                                                                                                   
    AUDIO : period time = 125000 us dir = 0                                                                                                                     
    queue id:65538                                                                                                                                              
    ***************************************                                                                                                                     
    APPROPHO AEW TRIAL VERSION !!!                                                                                                                              
    APPROPHO AEW DATE LINE 2011/6                                                                                                                               
    ***************************************                                                                                                                     
    XXXXX DRV_imgsSetAgain() Error(0)                                                                                                                           
    ND Init                                                                                                                                                     
    ND:Day                                                                                                                                                      
    --->Chip init PASS                                                                                                                                          
    Mode:0,F:2,Q:-1                                                                                                                                             
    Enable APPRO_DBG Function @@@@@@@@@@@@@@@@@@@@@                                                                                                             
       usb      [success]                                                                                                                                       
       isapnp                                                                                                                                                   
       isapnp   [success]                                                                                                                                       
       ide                                                                                                                                                      
       ide      [success]                                                                                                                                       
       input                                                                                                                                                    
    ROI DEBUG CONFIG: 0                                                                                                                                         
                                                                                                                                                                
    AEW TYPE DEBUG VALUE: 3                                                                                                                                     
    day_night = 0                                                                                                                                               
    GBCE DEBUG VALUE: 0                                                                                                                                         
                                                                                                                                                                
    FeatureMask: NONE.                                                                                                                                          
       input    [success]                                                                                                                                       
       scsi                                                                                                                                                     
       scsi     [success]                                                                                                                                       
    done.                                                                                                                                                       
    Starting portmap daemon: portmap.                                                                                                                           
    Starting internet superserver: inetd.                                                                                                                       
    io scheduler deadline registered                                                                                                                            
    io scheduler cfq registered                                                                                                                                 
    TI DaVinci EMAC: kernel boot params Ethernet address: 00:0C:0C:A0:04:B5                                                                                     
     sbulla: unknown partition table                                                                                                                            
    Installing knfsd (copyright (C) 1996 okir@monad.swb.de).                                                                                                    
    loop: loaded (max 8 devices)                                                                                                                                
    tun: Universal TUN/TAP device driver, 1.6                                                                                                                   
    tun: (C) 1999-2004 Max Krasnyansky <maxk@qualcomm.com>                                                                                                      
    CSLIP: code copyright 1989 Regents of the University of California                                                                                          
    netconsole: not configured, aborting                                                                                                                        
    PPP generic driver version 2.4.2                                                                                                                            
    PPP Deflate Compression module registered                                                                                                                   
    Davinci EMAC MII Bus: probed                                                                                                                                
    MAC address is 00:0C:0C:A0:04:B5                                                                                                                            
    TI DaVinci EMAC Linux version updated 4.0                                                                                                                   
    davinci-mmc davinci-mmc.0: Supporting 4-bit mode                                                                                                            
    davinci-mmc davinci-mmc.0: Using DMA mode                                                                                                                   
    usbcore: registered new driver usbfs                                                                                                                        
    usbcore: registered new driver hub                                                                                                                          
    musb_hdrc: version 6.0, cppi-dma, peripheral, debug=0                                                                                                       
    musb_hdrc musb_hdrc: No DMA interrupt line                                                                                                                  
    musb_hdrc: USB Peripheral mode controller at c38fa000 using DMA, IRQ 12                                                                                     
    Loading iSCSI transport class v1.1-646.<5>iscsi: registered transport (tcp)                                                                                 
     sbulla: unknown partition table                                                                                                                            
    mkdosfs 3.0.6 (04 Oct 2009)                                                                                                                                 
    unable to get drive geometry, using default 255/63                                                                                                          
    /dev/sbulla has 255 heads and 63 sectors per track,                                                                                                         
    logical sector size is 512,                                                                                                                                 
    using 0xf8 media descriptor, with 1024 sectors;                                                                                                             
    file system has 2 12-bit FATs and 4 sectors per cluster.                                                                                                    
    FAT size is 1 sector, and provides 247 clusters.                                                                                                            
    Root directory contains 512 slots.                                                                                                                          
    Volume ID is 62eeb10f, no volume label.                                                                                                                     
    queue id:0                                                                                                                                                  
    umount: /mnt/mmc: not mounted                                                                                                                               
    killall: dhcpcd: no process killed                                                                                                                          
    rm: cannot remove `/var/run/dhcpcd-eth0.pid': No such file or directory                                                                                     
    net_search_gateway:eth0, 20A, 0, 1                                                                                                                          
    dns=192.168.1.1                                                                                                                                             
    net_search_gateway:eth0, 20A, 0, 1                                                                                                                          
    net_search_gateway:eth0, 0, 102020A, 3                                                                                                                      
    dns=192.168.1.1                                                                                                                                             
    ERROR: Module g_file_storage does not exist in /proc/modules                                                                                                
    g_file_storage gadget: File-backed Storage Gadget, version: 28 November 2005                                                                                
    g_file_storage gadget: Number of LUNs=1                                                                                                                     
    g_file_storage gadget-lun0: ro=0, file: /dev/sbulla                                                                                                         
    system_server/538[CPU#0]: BUG in local_bh_enable at kernel/softirq.c:196                                                                                    
    ApproDrvInit: 2                                                                                                                                             
    ApproDrvInit: 6                                                                                                                                             
    queue id:98307                                                                                                                                              
    Initializing...                                                                                                                                             
    ApproDrvInit: 8                                                                                                                                             
    queue id:98307                                                                                                                                              
    ApproDrvInit: 3                                                                                                                                             
    queue id:98307                                                                                                                                              
    queue id:0                                                                                                                                                  
    queue id:32769                                                                                                                                              
    INIT: Entering runlevel: 3                                                                                                                                  
    ApproDrvInit: 9                                                                                                                                             
    queue id:98307                                                                                                                                              
    Initializing...                                                                                                                                             
    ApproDrvInit: 10                                                                                                                                            
    queue id:98307                                                                                                                                              
    Initializing...                                                                                                                                             
    ...done initializing                                                                                                                                        
    Play this stream using the URL:                                                                                                                             
            rtsp://10.2.141.117:8554/mpeg4                                                                                                                      
    queue id:98307                                                                                                                                              
    Initializing...                                                                                                                                             
    ...done initializing                                                                                                                                        
    Play this stream using the URL:                                                                                                                             
            rtsp://10.2.141.117/mpeg4                                                                                                                           
    ...done initializing                                                                                                                                        
    Play this stream using the URL:                                                                                                                             
            rtsp://10.2.141.117:8557/h264                                                                                                                       
    ...done initializing                                                                                                                                        
    Play this stream using the URL:                                                                                                                             
            rtsp://10.2.141.117:8556/h264                                                                                                                       
    Initializing...                                                                                                                                             
    ...done initializing                                                                                                                                        
    Play this stream using the URL:                                                                                                                             
            rtsp://10.2.141.117:8555/mjpeg                                                                                                                      
    queue id:0                                                                                                                                                  
    [03/Dec/2010:03:38:25 +0000] boa: server version Boa/0.94.13                                                                                                
    [03/Dec/2010:03:38:25 +0000] boa: server built Jul 14 2010 at 16:05:12.                                                                                     
    [03/Dec/2010:03:38:25 +0000] boa: starting server pid=814, port 80                                                                                          
    UDPString=uuid:Upnp-TVEmulator-1_0-00_0043158699</UDN>                                                                                                      
                                                                                                                                                                
    Upnp port is 0                                                                                                                                              
    UPnP Initialized OK ip=10.2.141.117, port=49152                                                                                                             
    desc_doc_url = http://10.2.141.117/tvdevicedesc.xml                                                                                                         
    error code = 0                                                                                                                                              
    device advertisement succeed.                                                                                                                               
                                                                                                                                                                
    MontaVista(R) Linux(R) Professional Edition 5.0.0 (0702774)                                                                                                 
                                                                                                                                                                
    DM36x_IPNC login: Audio disabled!                                                                                                                           
    Audio disabled!                                                                                                                                             
    Audio disabled!                                                                                                                                             
    Audio disabled!                                                                                                                                             
    Audio disabled!                                                                                                                                             
    Audio Alarm!!                                                                                                                                               
    Audio Alarm!!                                                                                                                                               
    Audio Alarm!!                                                                                                                                               
    Audio Alarm!!                                                                                                                                               
    Audio Alarm!!                                                                                                                                               
                                                                                                                                                                
    MontaVista(R) Linux(R) Professional Edition 5.0.0 (0702774)                                                                                                 
                                                                                                                                                                
    DM36x_IPNC login:                                                                                                                                           
     Module   | Avg Time/Frame | Frame-rate | Total time | Total Frames |                                                                                       
     CAPTURE  |          41.99 |      23.82 |      37829 |          901 |                                                                                       
     IPIPE    |          31.65 |      31.60 |      28515 |          901 |                                                                                       
     RESIZE   |           4.97 |     201.16 |       4479 |          901 |                                                                                       
     ENCODE0  |          16.63 |      60.14 |      14964 |          900 |                                                                                       
     STREAM   |           0.29 |    3488.37 |        258 |          900 |                                                                                       
     FACE.D   |          12.48 |      80.10 |        387 |           31 |                                                                                       
     AEWB     |           3.24 |     308.40 |       3677 |         1134 |                                                                                       
                                                                                                                                                                

  • Hi Anshuman,

    Do you have any news on this issue?

     

    Regards,

    Mahendra Kumar

  • Hi,

    Looking at the log below, you can see that sensor fps is set to 24 and that is the reason why you are seeing a slowed framerate. Rest of the system is running much more faster. You can increase the "sensorFPS" in the avserverUI.c

    Mahendra kumar Angamuthu Ganesan said:
    ############OPEN###########                                                                                                                                 
     Sensor Mode Info,                                                                                                                                          
     Width      = 2024                                                                                                                                          
     Height     = 1140                                                                                                                                          
     fps        =   24                                                                                                                                          
     Bin Enable =    1                                                                                                                                          
                                                                                                                                                                
     Sensor Frame Timing Info,                                                                                                                                  
     fps                  = 24                                                                                                                                  
     t_frame (ns)         = 41666668.000000                                                                                                                     
     t_row   (ns)         = 30458.333984                                                                                                                        
     t_pclk  (ns)         = 10.416667                                                                                                                           
     W                    = 2024                                                                                                                                
     H                    = 1140                                                                                                                                
     SW                   = 1406                                                                                                                                
     SD                   = 0                                                                                                                                   
     HB                   = 450                                                                                                                                 
     VB                   = 227                                                                                                                                 
     HBmin                = 450                                                                                                                                 
     VBmin                = 9                                                                                                                                   
     f_pclk               = 96000000                                                                                                                            
     shutterOverhead (ns) = 4437.500000                                                                                                                         
     col_size             = 2024                                                                                                                                
     row_size             = 1140                                                                                                                                
     col_bin              = 0                                                                                                                                   
     row_bin              = 0                                                                                                                                   
     col_start            = 88                                                                                                                                  
     row_start            = 276                                                                                                                                 
     pll_M                = 16                                                                                                                                  
     pll_N                = 1                                                                                                                                   
     pll_DIV              = 1                                                                                                                                   
                                                                                                                                                                
    ############reset###########      

    Regards,

    Anshuman

  • hi Anshuman,

    we are facing the same problem.

    i want to ask if it is work for you.

    we've done many tests use dm365 resize, such as d1, vga, cif, qvga, qcif   to 800x480, all is ok except qcif failed with timeout error.

    if we change m=10, n=240 as we have done on the other resolutions , the timeout error gone.but the dist yuv is not ok.

    we'd like to ask for advices.

    thanks.

    regards, Mike