Part Number: TDA2EVM5777
Other Parts Discussed in Thread: DRA742, PMP, DRA752
Tool/software: Linux
Hello .
I am trying to boot the TDA2xx with SD BOOT image, the log is as follows
U-Boot SPL 2016.05-00013-g3331a8a-dirty (Mar 29 2019 - 16:40:23)
DRA752-GP ES2.0
no pinctrl for hs200_1_8v
no pinctrl for ddr_1_8v
** First descriptor is NOT a primary desc on 1:1 **
*** Warning - bad CRC, using default environment
Trying to boot from MMC1
reading dra7-ipu2-fw.lzop
spl_load_file_fat: error reading file dra7-ipu2-fw.lzop, err - -1
spl: error reading image dra7-ipu2-fw.lzop, err - -1
Error loading remotecore IPU2!,Continuing with boot ...
reading dra7-dsp1-fw.lzop
spl_load_file_fat: error reading file dra7-dsp1-fw.lzop, err - -1
spl: error reading image dra7-dsp1-fw.lzop, err - -1
Error loading remotecore DSP1!,Continuing with boot ...
reading dra7-dsp2-fw.lzop
spl_load_file_fat: error reading file dra7-dsp2-fw.lzop, err - -1
spl: error reading image dra7-dsp2-fw.lzop, err - -1
Error loading remotecore DSP2!,Continuing with boot ...
reading dra7-ipu1-fw.lzop
spl_load_file_fat: error reading file dra7-ipu1-fw.lzop, err - -1
spl: error reading image dra7-ipu1-fw.lzop, err - -1
Error loading remotecore IPU1!,Continuing with boot ...
*** Warning - bad CRC, using default environment
reading u-boot.img
reading u-boot.img
reading u-boot.img
reading u-boot.img
U-Boot 2016.05-00013-g3331a8a-dirty (Mar 29 2019 - 16:40:23 +0530)
CPU : DRA752-GP ES2.0
Model: TI DRA742
Board: DRA74x EVM REV H.0
DRAM: 4 GiB
MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1
** First descriptor is NOT a primary desc on 1:1 **
*** Warning - bad CRC, using default environment
GUID Partition Table Header signature is wrong: 0x0 != 0x5452415020494645
part_get_info_efi: *** ERROR: Invalid GPT ***
GUID Partition Table Header signature is wrong: 0x0 != 0x5452415020494645
part_get_info_efi: *** ERROR: Invalid Backup GPT ***
ERROR: cannot find partition: 'userdata'
at arch/arm/cpu/armv7/omap-common/utils.c:199/mmc_get_part_size()
Warning: fastboot.userdata_size: unable to calc
SCSI: SATA link 0 timeout.
AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode
flags: 64bit ncq stag pm led clo only pmp pio slum part ccc apst
scanning bus for devices...
Found 0 device(s).
Net:
Warning: ethernet@48484000 using MAC address from ROM
eth0: ethernet@48484000
Hit any key to stop autoboot: 0
## Error: "board_findfdt" not defined
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
reading boot.scr
** Unable to read file boot.scr **
reading uEnv.txt
215 bytes read in 2 ms (104.5 KiB/s)
Loaded env from uEnv.txt
Importing environment from mmc0 ...
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
3560304 bytes read in 112 ms (30.3 MiB/s)
106947 bytes read in 9 ms (11.3 MiB/s)
Booting from mmc0 ...
Kernel image @ 0x82000000 [ 0x000000 - 0x365370 ]
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
Loading Device Tree to 8ffe2000, end 8ffff1c2 ... OK
Starting kernel ...
[ 0.000000] Booting Linux on physical CPU 0x0
[ 0.000000] Initializing cgroup subsys cpuset
[ 0.000000] Initializing cgroup subsys cpu
[ 0.000000] Initializing cgroup subsys cpuacct
[ 0.000000] Linux version 4.4.84-00034-gaa42c96 (root@lnmiit-HP-ProDesk-400-G2-MT) (gcc version 5.3.1 20160113 (Linaro GCC 5.3-2016.02) ) #4 SMP PREEMPT Fri Mar 29 16:41:33 IST 2019
[ 0.000000] CPU: ARMv7 Processor [412fc0f2] revision 2 (ARMv7), cr=30c5387d
[ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, PIPT instruction cache
[ 0.000000] Machine model: TI DRA742
[ 0.000000] Reserved memory: created DMA memory pool at 0x0000000040300000, size 3 MiB
[ 0.000000] Reserved memory: initialized node cmem@40300000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: regions without no-map are not yet supported
[ 0.000000] Reserved memory: created CMA memory pool at 0x0000000099000000, size 80 MiB
[ 0.000000] Reserved memory: initialized node ipu2_cma@95800000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created CMA memory pool at 0x000000009e000000, size 32 MiB
[ 0.000000] Reserved memory: initialized node ipu1_cma@9d000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: regions without no-map are not yet supported
[ 0.000000] Reserved memory: created CMA memory pool at 0x00000000a1000000, size 32 MiB
[ 0.000000] Reserved memory: initialized node dsp1_cma@99000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: created CMA memory pool at 0x00000000a3000000, size 32 MiB
[ 0.000000] Reserved memory: initialized node dsp2_cma@9f000000, compatible id shared-dma-pool
[ 0.000000] Reserved memory: regions without no-map are not yet supported
[ 0.000000] Reserved memory: created DMA memory pool at 0x00000000a9000000, size 32 MiB
[ 0.000000] Reserved memory: initialized node cmem@A9000000, compatible id shared-dma-pool
[ 0.000000] cma: Reserved 24 MiB at 0x00000000be400000
[ 0.000000] Forcing write-allocate cache policy for SMP
[ 0.000000] Memory policy: Data cache writealloc
[ 0.000000] OMAP4: Map 0x00000000bfd00000 to fe600000 for dram barrier
[ 0.000000] DRA752 ES2.0
[ 0.000000] PERCPU: Embedded 11 pages/cpu @ef62a000 s14912 r8192 d21952 u45056
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 251456
[ 0.000000] Kernel command line: console=ttyO0,115200n8 vram=16M root=/dev/nfs rw nfsroot=172.24.210.101:/adasuser/shiju/ADAS/ti_components/os_tools/linux/targetfs rootwait ip=dhcp mem=1024M
[ 0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
[ 0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Memory: 394148K/1012736K available (6635K kernel code, 320K rwdata, 2392K rodata, 336K init, 290K bss, 413788K reserved, 204800K cma-reserved, 234496K highmem)
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB)
[ 0.000000] vmalloc : 0xf0800000 - 0xff800000 ( 240 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xf0000000 ( 768 MB)
[ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB)
[ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB)
[ 0.000000] .text : 0xc0008000 - 0xc08d902c (9029 kB)
[ 0.000000] .init : 0xc08da000 - 0xc092e000 ( 336 kB)
[ 0.000000] .data : 0xc092e000 - 0xc097e120 ( 321 kB)
[ 0.000000] .bss : 0xc0980000 - 0xc09c8800 ( 290 kB)
[ 0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] Build-time adjustment of leaf fanout to 32.
[ 0.000000] NR_IRQS:16 nr_irqs:16 16
[ 0.000000] ti_dt_clocks_register: failed to lookup clock node gmac_gmii_ref_clk_div
[ 0.000000] OMAP clockevent source: timer1 at 32786 Hz
[ 0.000000] Architected cp15 timer(s) running at 6.14MHz (phys).
[ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x16af5adb9, max_idle_ns: 440795202250 ns
[ 0.000005] sched_clock: 56 bits at 6MHz, resolution 162ns, wraps every 4398046511023ns
[ 0.000016] Switching to timer-based delay loop, resolution 162ns
[ 0.000329] clocksource: 32k_counter: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 58327039986419 ns
[ 0.000337] OMAP clocksource: 32k_counter at 32768 Hz
[ 0.000779] Console: colour dummy device 80x30
[ 0.000795] WARNING: Your 'console=ttyO0' has been replaced by 'ttyS0'
[ 0.000801] This ensures that you still see kernel messages. Please
[ 0.000806] update your kernel commandline.
[ 0.000820] Calibrating delay loop (skipped), value calculated using timer frequency.. 12.29 BogoMIPS (lpj=61475)
[ 0.000833] pid_max: default: 32768 minimum: 301
[ 0.000930] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.000940] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.001485] Initializing cgroup subsys io
[ 0.001501] Initializing cgroup subsys memory
[ 0.001525] Initializing cgroup subsys devices
[ 0.001538] Initializing cgroup subsys freezer
[ 0.001548] Initializing cgroup subsys perf_event
[ 0.001559] Initializing cgroup subsys pids
[ 0.001585] CPU: Testing write buffer coherency: ok
[ 0.001786] /cpus/cpu@0 missing clock-frequency property
[ 0.001802] /cpus/cpu@1 missing clock-frequency property
[ 0.001812] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
[ 0.001850] Setting up static identity map for 0x80008380 - 0x800083e0
[ 0.080061] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
[ 0.080129] Brought up 2 CPUs
[ 0.080141] SMP: Total of 2 processors activated (24.59 BogoMIPS).
[ 0.080147] CPU: All CPU(s) started in HYP mode.
[ 0.080153] CPU: Virtualization extensions available.
[ 0.080531] devtmpfs: initialized
[ 0.109198] VFP support v0.3: implementor 41 architecture 4 part 30 variant f rev 0
[ 0.110173] omap_hwmod: l3_main_2 using broken dt data from ocp
[ 0.313944] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[ 0.313968] futex hash table entries: 512 (order: 3, 32768 bytes)
[ 0.318408] pinctrl core: initialized pinctrl subsystem
[ 0.319280] NET: Registered protocol family 16
[ 0.320236] DMA: preallocated 256 KiB pool for atomic coherent allocations
[ 0.350238] cpuidle: using governor ladder
[ 0.380261] cpuidle: using governor menu
[ 0.388830] OMAP GPIO hardware version 0.1
[ 0.395304] irq: no irq domain found for /ocp/l4@4a000000/scm@2000/pinmux@1400 !
[ 0.411928] omap-gpmc 50000000.gpmc: GPMC revision 6.0
[ 0.411941] gpmc_mem_init: disabling cs 0 mapped at 0x0-0x1000000
[ 0.420541] hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.
[ 0.420551] hw-breakpoint: maximum watchpoint size is 8 bytes.
[ 0.421015] omap4_sram_init:Unable to allocate sram needed to handle errata I688
[ 0.421025] omap4_sram_init:Unable to get sram pool needed to handle errata I688
[ 0.421605] OMAP DMA hardware revision 0.0
[ 0.461551] omap-dma-engine 4a056000.dma-controller: OMAP DMA engine driver (LinkedList1/2/3 supported)
[ 0.462709] edma 43300000.edma: memcpy is disabled
[ 0.467498] edma 43300000.edma: TI EDMA DMA engine driver
[ 0.471906] omap-iommu 40d01000.mmu: 40d01000.mmu registered
[ 0.472085] omap-iommu 40d02000.mmu: 40d02000.mmu registered
[ 0.472246] omap-iommu 58882000.mmu: 58882000.mmu registered
[ 0.472403] omap-iommu 55082000.mmu: 55082000.mmu registered
[ 0.472697] omap-iommu 41501000.mmu: 41501000.mmu registered
[ 0.472881] omap-iommu 41502000.mmu: 41502000.mmu registered
[ 0.475878] palmas 0-0058: IRQ missing: skipping irq request
[ 0.491270] palmas 0-0058: Muxing GPIO 2e, PWM 0, LED 0
[ 0.563495] pcf857x 0-0020: probed
[ 0.564072] pcf857x 0-0021: probed
[ 0.564223] omap_i2c 48070000.i2c: bus 0 rev0.12 at 400 kHz
[ 0.564628] omap_i2c 48060000.i2c: bus 2 rev0.12 at 400 kHz
[ 0.564826] media: Linux media interface: v0.10
[ 0.564878] Linux video capture interface: v2.00
[ 0.564921] pps_core: LinuxPPS API ver. 1 registered
[ 0.564928] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
[ 0.564951] PTP clock support registered
[ 0.564994] EDAC MC: Ver: 3.0.0
[ 0.565745] omap-mailbox 48840000.mailbox: omap mailbox rev 0x400
[ 0.566039] omap-mailbox 48842000.mailbox: omap mailbox rev 0x400
[ 0.566386] Advanced Linux Sound Architecture Driver Initialized.
[ 0.567263] clocksource: Switched to clocksource arch_sys_counter
[ 0.577959] NET: Registered protocol family 2
[ 0.578455] TCP established hash table entries: 8192 (order: 3, 32768 bytes)
[ 0.578518] TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
[ 0.578643] TCP: Hash tables configured (established 8192 bind 8192)
[ 0.578691] UDP hash table entries: 512 (order: 2, 16384 bytes)
[ 0.578722] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
[ 0.578927] NET: Registered protocol family 1
[ 0.579192] RPC: Registered named UNIX socket transport module.
[ 0.579201] RPC: Registered udp transport module.
[ 0.579208] RPC: Registered tcp transport module.
[ 0.579214] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.580226] hw perfevents: enabled with armv7_cortex_a15 PMU driver, 7 counters available
[ 0.590301] squashfs: version 4.0 (2009/01/31) Phillip Lougher
[ 0.590966] NFS: Registering the id_resolver key type
[ 0.590991] Key type id_resolver registered
[ 0.590998] Key type id_legacy registered
[ 0.591067] ntfs: driver 2.1.32 [Flags: R/O].
[ 0.592380] bounce: pool size: 64 pages
[ 0.592531] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 247)
[ 0.592549] io scheduler noop registered
[ 0.592564] io scheduler deadline registered
[ 0.592599] io scheduler cfq registered (default)
[ 0.597537] pinctrl-single 4a003400.pinmux: 282 pins at pa fc003400 size 1128
[ 0.600711] PCI host bridge /ocp/axi@0/pcie_rc@51000000 ranges:
[ 0.600723] No bus range found for /ocp/axi@0/pcie_rc@51000000, using [bus 00-ff]
[ 0.600756] IO 0x20003000..0x20012fff -> 0x00000000
[ 0.600776] MEM 0x20013000..0x2fffffff -> 0x20013000
[ 0.630678] dra7-pcie 51000000.pcie_rc: link is not up
[ 0.630852] dra7-pcie 51000000.pcie_rc: PCI host bridge to bus 0000:00
[ 0.630865] pci_bus 0000:00: root bus resource [bus 00-ff]
[ 0.630875] pci_bus 0000:00: root bus resource [io 0x0000-0xffff]
[ 0.630885] pci_bus 0000:00: root bus resource [mem 0x20013000-0x2fffffff]
[ 0.631280] PCI: bus0: Fast back to back transfers disabled
[ 0.631403] PCI: bus1: Fast back to back transfers enabled
[ 0.631486] pci 0000:00:00.0: BAR 0: assigned [mem 0x20100000-0x201fffff]
[ 0.631501] pci 0000:00:00.0: BAR 1: assigned [mem 0x20020000-0x2002ffff]
[ 0.631513] pci 0000:00:00.0: PCI bridge to [bus 01]
[ 0.631732] pcieport 0000:00:00.0: Signaling PME through PCIe PME interrupt
[ 0.692282] Serial: 8250/16550 driver, 10 ports, IRQ sharing disabled
[ 0.695689] 4806a000.serial: ttyS0 at MMIO 0x4806a000 (irq = 301, base_baud = 3000000) is a 8250
[ 1.712179] console [ttyS0] enabled
[ 1.716576] 4806c000.serial: ttyS1 at MMIO 0x4806c000 (irq = 302, base_baud = 3000000) is a 8250
[ 1.726261] 48020000.serial: ttyS2 at MMIO 0x48020000 (irq = 303, base_baud = 3000000) is a 8250
[ 1.736298] [drm] Initialized drm 1.1.0 20060810
[ 1.741843] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
[ 1.748506] [drm] No driver support for vblank timestamp query.
[ 1.754637] [drm] Initialized vdrm 1.0.0 20110917 on minor 0
[ 1.767637] loop: module loaded
[ 1.771173] vmemexp device MAJOR num = 245
[ 1.775301] vmemexp class registered
[ 1.779041] /dev/vmemexp device registered
[ 1.783155] ioctl DBUFIOC_EXPORT_VIRTMEM = -1072899120
[ 1.788870] nand: No NAND device found
[ 1.792641] omap2-nand 8000000.nand: scan failed, may be bus-width mismatch
[ 1.802620] m25p80 spi32766.0: s25fl256s1 (32768 Kbytes)
[ 1.808041] 7 ofpart partitions found on MTD device spi32766.0
[ 1.813900] Creating 7 MTD partitions on "spi32766.0":
[ 1.819081] 0x000000000000-0x000000040000 : "QSPI.SPL"
[ 1.825176] 0x000000040000-0x000000140000 : "QSPI.u-boot"
[ 1.831531] 0x000000140000-0x0000001c0000 : "QSPI.u-boot-spl-os"
[ 1.838476] 0x0000001c0000-0x0000001d0000 : "QSPI.u-boot-env"
[ 1.845155] 0x0000001d0000-0x0000001e0000 : "QSPI.u-boot-env.backup1"
[ 1.852559] 0x0000001e0000-0x0000009e0000 : "QSPI.kernel"
[ 1.858895] 0x0000009e0000-0x000002000000 : "QSPI.file-system"
[ 1.866675] libphy: Fixed MDIO Bus: probed
[ 1.917297] davinci_mdio 48485000.mdio: davinci mdio revision 1.6
[ 1.923421] davinci_mdio 48485000.mdio: detected phy mask fffffff3
[ 1.933856] libphy: 48485000.mdio: probed
[ 1.937907] davinci_mdio 48485000.mdio: phy[2]: device 48485000.mdio:02, driver unknown
[ 1.945947] davinci_mdio 48485000.mdio: phy[3]: device 48485000.mdio:03, driver unknown
[ 1.954629] cpsw 48484000.ethernet: Detected MACID = f0:b5:d1:0f:05:82
[ 1.961290] cpsw 48484000.ethernet: cpts: overflow check period 800
[ 1.968261] cpsw 48484000.ethernet: cpsw: Detected MACID = f0:b5:d1:0f:05:83
[ 1.976866] mousedev: PS/2 mouse device common for all mice
[ 1.983052] i2c /dev entries driver
[ 1.991784] omap_hsmmc 4809c000.mmc: Got CD GPIO
[ 1.997418] omap_hsmmc 480b4000.mmc: no pinctrl state for sdr25 mode
[ 2.003805] omap_hsmmc 480b4000.mmc: no pinctrl state for sdr12 mode
[ 2.010362] evm_3v3_sw: supplied by sysen1
[ 2.091043] mmc0: MAN_BKOPS_EN bit is not set
[ 2.102875] mmc0: new HS200 MMC card at address 0001
[ 2.118363] mmcblk0: mmc0:0001 MMC08G 7.25 GiB
[ 2.133156] mmcblk0boot0: mmc0:0001 MMC08G partition 1 8.00 MiB
[ 2.139368] mmcblk0boot1: mmc0:0001 MMC08G partition 2 8.00 MiB
[ 2.169083] ledtrig-cpu: registered to indicate activity on CPUs
[ 2.177616] aic_dvdd: supplied by evm_3v3_sw
[ 2.183532] davinci-mcasp 4847c000.mcasp: invalid tdm slots: 0
[ 2.191046] NET: Registered protocol family 10
[ 2.206300] sit: IPv6 over IPv4 tunneling driver
[ 2.211512] NET: Registered protocol family 17
[ 2.216208] Key type dns_resolver registered
[ 2.220653] omap_voltage_late_init: Voltage driver support not added
[ 2.227554] Adding alias for supply vdd,cpu0 -> vdd,4a003b20.oppdm
[ 2.233765] Adding alias for supply vbb,cpu0 -> vbb,4a003b20.oppdm
[ 2.240515] Adding alias for supply vdd,cpu0 -> vdd,4a003b20.oppdm
[ 2.246723] Adding alias for supply vbb,cpu0 -> vbb,4a003b20.oppdm
[ 2.254954] Power Management for TI OMAP4+ devices.
[ 2.260059] Registering SWP/SWPB emulation handler
[ 2.265795] dmm 4e000000.dmm: workaround for errata i878 in use
[ 2.273096] dmm 4e000000.dmm: initialized all PAT entries
[ 2.279219] [drm] Initialized omapdrm 1.0.0 20110917 on minor 1
[ 2.296135] omap_hsmmc 4809c000.mmc: Got CD GPIO
[ 2.338593] asoc-simple-card sound0: tlv320aic3x-hifi <-> 48468000.mcasp mapping ok
[ 2.358250] input: gpio_keys as /devices/platform/gpio_keys/input/input0
[ 2.367342] hctosys: unable to open rtc device (rtc0)
[ 2.380881] net eth0: initializing cpsw version 1.15 (0)
[ 2.386239] net eth0: initialized cpsw ale version 1.4
[ 2.391429] net eth0: ALE Table size 1024
[ 2.402661] net eth0: phy found : id is : 0x20005c7a
[ 2.413666] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
[ 2.419574] net eth1: initializing cpsw version 1.15 (0)
[ 2.431782] net eth1: phy found : id is : 0x20005c7a
[ 2.441425] IPv6: ADDRCONF(NETDEV_UP): eth1: link is not ready
[ 2.587100] mmc2: host does not support reading read-only switch, assuming write-enable
[ 2.599108] mmc2: new ultra high speed DDR50 SDHC card at address aaaa
[ 2.605956] mmcblk1: mmc2:aaaa SS08G 7.40 GiB
[ 2.620347] mmcblk1: p1 p2
[ 4.404861] cpsw 48484000.ethernet eth0: Link is Up - 100Mbps/Full - flow control rx/tx
[ 4.412952] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
[ 4.427289] Sending DHCP requests ., OK
[ 5.167280] IP-Config: Got DHCP answer from 172.22.16.1, my address is 172.22.16.86
[ 5.180742] IP-Config: Complete:
[ 5.183989] device=eth0, hwaddr=f0:b5:d1:0f:05:82, ipaddr=172.22.16.86, mask=255.255.255.0, gw=172.22.16.1
[ 5.194146] host=172.22.16.86, domain=, nis-domain=(none)
[ 5.200023] bootserver=0.0.0.0, rootserver=172.24.210.101, rootpath=
[ 5.206666] nameserver0=172.22.2.66, nameserver1=14.139.5.5, nameserver2=8.8.8.8
[ 5.214892] evm_1v8: disabling
[ 5.218002] aic_dvdd: disabling
[ 5.221158] vmmcwl_fixed: disabling
[ 5.224888] ldousb: disabling
[ 5.228432] ALSA device list:
[ 5.231413] #0: DRA7xx-EVM
Booting stops here,
i do want to know how do we have to edit the uenv.txt, i mean which server ip and root path it should point to.
Regards
Rather