This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/TDA2EVM5777: pSystemVideoFrameBuffer->bufAddr[0] != NULL : failed !!!

Part Number: TDA2EVM5777


Tool/software: Linux

Hi :

   i  am  using   SDK_VISION_03_04_00_00   ,  build  is  ok   !

 but  run  the  program    have    some  problem

[HOST] [DSP1  ]     44.332062 s:  ALG_FRAMECOPY: DMA: Allocated CH (TCC) = 0 (0)
 [HOST] [DSP1  ]     44.333129 s:  Assertion @ Line: 395 in framecopy/frameCopyLink_algPlugin.c: pSystemVideoFrameBuffer->bufAddr[0] != NULL : failed !!!
 [HOST] [IPU2  ]     44.332245 s:
 [HOST] [IPU2  ]     44.332336 s:  ### XDC ASSERT - ERROR CALLBACK START ###
 [HOST] [IPU2  ]     44.332397 s:
 [HOST] [IPU2  ]     44.332519 s: out of memory: handle=0x99e0a4a4, size=5898240
 [HOST] [IPU2  ]     44.332641 s:
 [HOST] [IPU2  ]     44.332702 s:  ### XDC ASSERT - ERROR CALLBACK END ###
 [HOST] [IPU2  ]     44.332763 s:

what  is  the  problem?

THANKS

Shuai