Hi
I'd like a thread in my application to wake up at a certain period and do some work. The amount of work will vary so I do not want to sleep for some fixed amount of time. The desired rate is 10-60 Hz.
This is between 16 and 100 ms. It's a soft requirement in that a missed period does no harm to the application.
Are there any timing services available?
Also, I've been using PThreads. I haven't yet messed with the real-time scheduler in Monte Vista. Can I make one of these threads real-time? Or will the regular scheduler work OK for this?
Thanks,
Ken