Tool/software: Linux
I have a Beaglebone black and I am trying to build a custom Os using buildroot. I am using the default configuration provided for beaglebone using the following command:
make beaglebone_defconfig make
I am following this link as a guide.
I have an Sd card and I have created 2 Partitions.
The Partition 1 is a boot partition and partition 2 is a rootfs partition.
Partition 1 is created using the following command:
sudo mkfs.vfat -F 32 -n boot /dev/mmcblk0p1
and it is of size 128Mb. Partition 1 consists of the following files:
- MLO
- uEnv.txt
- u-boot.img
- zImage
- am335x-boneblack.dtb
Partition 2 is created using:
sudo mkfs.ext4 -L rootfs -E sdcard /dev/mmcblk0p2
Now when I boot the Beaglebone using Serial console I get following logs:
U-Boot SPL 2018.09-00002-g0b54a51eee (Sep 10 2018 - 19:41:39 -0500) Trying to boot from MMC2 Loading Environment from EXT4... ** Unable to use mmc 0:1 for loading the env ** U-Boot 2018.09-00002-g0b54a51eee (Sep 10 2018 - 19:41:39 -0500), Build: jenkins-github_Bootloader-Builder-65 CPU : AM335X-GP rev 2.1 I2C: ready DRAM: 512 MiB No match for driver 'omap_hsmmc' No match for driver 'omap_hsmmc' Some drivers were not found Reset Source: Power-on reset has occurred. RTC 32KCLK Source: External. MMC: OMAP SD/MMC: 0, OMAP SD/MMC: 1 Loading Environment from EXT4... ** Unable to use mmc 0:1 for loading the env ** Board: BeagleBone Black <ethaddr> not set. Validating first E-fuse MAC BeagleBone Black: BeagleBone: cape eeprom: i2c_probe: 0x54: BeagleBone: cape eeprom: i2c_probe: 0x55: BeagleBone: cape eeprom: i2c_probe: 0x56: BeagleBone: cape eeprom: i2c_probe: 0x57: Net: eth0: MII MODE cpsw, usb_ether Press SPACE to abort autoboot in 2 seconds board_name=[A335BNLT] ... board_rev=[00C0] ... switch to partitions #0, OK mmc0 is current device SD/MMC found on device 0 switch to partitions #0, OK mmc0 is current device Scanning mmc 0:1... 36793 bytes read in 8 ms (4.4 MiB/s) gpio: pin 56 (gpio 56) value is 0 gpio: pin 55 (gpio 55) value is 0 gpio: pin 54 (gpio 54) value is 0 gpio: pin 53 (gpio 53) value is 1 switch to partitions #0, OK mmc0 is current device gpio: pin 54 (gpio 54) value is 1 Checking for: /uEnv.txt ... 376 bytes read in 2 ms (183.6 KiB/s) gpio: pin 55 (gpio 55) value is 1 Loaded environment from /uEnv.txt Importing environment from mmc ... Checking if uenvcmd is set ... gpio: pin 56 (gpio 56) value is 1 Running uenvcmd ... 5557120 bytes read in 357 ms (14.8 MiB/s) loading /am335x-boneblack.dtb ... 36793 bytes read in 5 ms (7 MiB/s) bootargs=console=ttyO0,115200n8 root=/dev/mmcblk0p2 rw rootfstype=ext4 rootwait ## Flattened Device Tree blob at 88000000 Booting using the fdt blob at 0x88000000 Loading Device Tree to 8fff4000, end 8fffffb8 ... OK Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0 [ 0.000000] Linux version 4.14.40 (local@local-server) (gcc version 7.4.0 (Buildroot 2019.05-git-00541-gdde9d60)) #2 SMP Tue Apr 2 18:46:25 IST 2019 [ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c5387d [ 0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache [ 0.000000] OF: fdt: Machine model: TI AM335x BeagleBone Black [ 0.000000] Memory policy: Data cache writeback [ 0.000000] cma: Reserved 16 MiB at 0x9e800000 [ 0.000000] CPU: All CPU(s) started in SVC mode. [ 0.000000] AM335X ES2.1 (sgx neon) [ 0.000000] percpu: Embedded 17 pages/cpu @df93c000 s40872 r8192 d20568 u69632 [ 0.000000] Built 1 zonelists, mobility grouping on. Total pages: 129412 [ 0.000000] Kernel command line: console=ttyO0,115200n8 root=/dev/mmcblk0p2 rw rootfstype=ext4 rootwait [ 0.000000] PID hash table entries: 2048 (order: 1, 8192 bytes) [ 0.000000] Dentry cache hash table entries: 65536 (order: 6, 262144 bytes) [ 0.000000] Inode-cache hash table entries: 32768 (order: 5, 131072 bytes) [ 0.000000] Memory: 479872K/522240K available (8192K kernel code, 817K rwdata, 2420K rodata, 1024K init, 7548K bss, 25984K reserved, 16384K cma-reserved, 0K highmem) [ 0.000000] Virtual kernel memory layout: [ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB) [ 0.000000] fixmap : 0xffc00000 - 0xfff00000 (3072 kB) [ 0.000000] vmalloc : 0xe0000000 - 0xff800000 ( 504 MB) [ 0.000000] lowmem : 0xc0000000 - 0xdfe00000 ( 510 MB) [ 0.000000] pkmap : 0xbfe00000 - 0xc0000000 ( 2 MB) [ 0.000000] modules : 0xbf000000 - 0xbfe00000 ( 14 MB) [ 0.000000] .text : 0xc0008000 - 0xc0900000 (9184 kB) [ 0.000000] .init : 0xc0c00000 - 0xc0d00000 (1024 kB) [ 0.000000] .data : 0xc0d00000 - 0xc0dcc7b8 ( 818 kB) [ 0.000000] .bss : 0xc0dce000 - 0xc152d054 (7549 kB) [ 0.000000] Running RCU self tests [ 0.000000] Hierarchical RCU implementation. [ 0.000000] RCU event tracing is enabled. [ 0.000000] RCU lockdep checking is enabled. [ 0.000000] RCU restricting CPUs from NR_CPUS=2 to nr_cpu_ids=1. [ 0.000000] RCU: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=1 [ 0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16 [ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts [ 0.000000] OMAP clockevent source: timer2 at 24000000 Hz [ 0.000018] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 89478484971ns [ 0.000048] clocksource: timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 79635851949 ns [ 0.000101] OMAP clocksource: timer1 at 24000000 Hz [ 0.000649] timer_probe: no matching timers found [ 0.001556] Console: colour dummy device 80x30 [ 0.001606] Lock dependency validator: Copyright (c) 2006 Red Hat, Inc., Ingo Molnar [ 0.001619] ... MAX_LOCKDEP_SUBCLASSES: 8 [ 0.001632] ... MAX_LOCK_DEPTH: 48 [ 0.001644] ... MAX_LOCKDEP_KEYS: 8191 [ 0.001656] ... CLASSHASH_SIZE: 4096 [ 0.001668] ... MAX_LOCKDEP_ENTRIES: 32768 [ 0.001680] ... MAX_LOCKDEP_CHAINS: 65536 [ 0.001692] ... CHAINHASH_SIZE: 32768 [ 0.001704] memory used by lock dependency info: 4655 kB [ 0.001717] per task-struct memory footprint: 1536 bytes [ 0.001752] Calibrating delay loop... 996.14 BogoMIPS (lpj=4980736) [ 0.078638] pid_max: default: 32768 minimum: 301 [ 0.079038] Security Framework initialized [ 0.079178] Mount-cache hash table entries: 1024 (order: 0, 4096 bytes) [ 0.079199] Mountpoint-cache hash table entries: 1024 (order: 0, 4096 bytes) [ 0.082304] CPU: Testing write buffer coherency: ok [ 0.083791] CPU0: thread -1, cpu 0, socket -1, mpidr 0 [ 0.085292] Setting up static identity map for 0x80100000 - 0x80100078 [ 0.085863] Hierarchical SRCU implementation. [ 0.087494] smp: Bringing up secondary CPUs ... [ 0.087520] smp: Brought up 1 node, 1 CPU [ 0.087537] SMP: Total of 1 processors activated (996.14 BogoMIPS). [ 0.087552] CPU: All CPU(s) started in SVC mode. [ 0.091459] devtmpfs: initialized [ 0.116646] random: get_random_u32 called from bucket_table_alloc+0xe4/0x23c with crng_init=0 [ 0.117615] VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3 [ 0.118377] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns [ 0.118447] futex hash table entries: 256 (order: 2, 16384 bytes) [ 0.120248] pinctrl core: initialized pinctrl subsystem [ 0.124538] NET: Registered protocol family 16 [ 0.131647] DMA: preallocated 256 KiB pool for atomic coherent allocations [ 0.217406] cpuidle: using governor menu [ 0.229343] OMAP GPIO hardware version 0.1 [ 0.253893] No ATAGs? [ 0.253919] hw-breakpoint: debug architecture 0x4 unsupported. [ 0.254230] omap4_sram_init:Unable to allocate sram needed to handle errata I688 [ 0.254251] omap4_sram_init:Unable to get sram pool needed to handle errata I688 [ 0.289499] edma 49000000.edma: TI EDMA DMA engine driver [ 0.294363] SCSI subsystem initialized [ 0.296055] omap_i2c 44e0b000.i2c: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/pinmux_i2c0_pins, deferring probe [ 0.296183] omap_i2c 4819c000.i2c: could not find pctldev for node /ocp/l4_wkup@44c00000/scm@210000/pinmux@800/pinmux_i2c2_pins, deferring probe [ 0.296465] pps_core: LinuxPPS API ver. 1 registered [ 0.296484] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it> [ 0.296544] PTP clock support registered [ 0.300654] clocksource: Switched to clocksource timer1 [ 0.434539] VFS: Disk quotas dquot_6.6.0 [ 0.434729] VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes) [ 0.458712] NET: Registered protocol family 2 [ 0.460661] TCP established hash table entries: 4096 (order: 2, 16384 bytes) [ 0.460768] TCP bind hash table entries: 4096 (order: 5, 147456 bytes) [ 0.461939] TCP: Hash tables configured (established 4096 bind 4096) [ 0.462371] UDP hash table entries: 256 (order: 2, 20480 bytes) [ 0.462569] UDP-Lite hash table entries: 256 (order: 2, 20480 bytes) [ 0.463329] NET: Registered protocol family 1 [ 0.465451] RPC: Registered named UNIX socket transport module. [ 0.465497] RPC: Registered udp transport module. [ 0.465512] RPC: Registered tcp transport module. [ 0.465527] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 0.467963] hw perfevents: no interrupt-affinity property for /pmu, guessing. [ 0.468954] hw perfevents: enabled with armv7_cortex_a8 PMU driver, 5 counters available [ 0.471612] audit: initializing netlink subsys (disabled) [ 0.474118] audit: type=2000 audit(0.470:1): state=initialized audit_enabled=0 res=1 [ 0.474447] workingset: timestamp_bits=14 max_order=17 bucket_order=3 [ 0.477146] NFS: Registering the id_resolver key type [ 0.477506] Key type id_resolver registered [ 0.477545] Key type id_legacy registered [ 0.477692] jffs2: version 2.2. (NAND) (SUMMARY) © 2001-2006 Red Hat, Inc. [ 0.484402] io scheduler noop registered [ 0.484435] io scheduler deadline registered [ 0.484561] io scheduler cfq registered (default) [ 0.484580] io scheduler mq-deadline registered [ 0.484596] io scheduler kyber registered [ 0.486649] pinctrl-single 44e10800.pinmux: 142 pins at pa f9e10800 size 568 [ 0.492083] Serial: 8250/16550 driver, 6 ports, IRQ sharing enabled [ 0.497651] omap_uart 44e09000.serial: no wakeirq for uart0 [ 0.498056] 44e09000.serial: ttyO0 at MMIO 0x44e09000 (irq = 30, base_baud = 3000000) is a OMAP UART0 [ 1.223666] console [ttyO0] enabled [ 1.255579] brd: module loaded [ 1.283987] loop: module loaded [ 1.289635] mtdoops: mtd device (mtddev=name/number) must be supplied [ 1.299291] libphy: Fixed MDIO Bus: probed [ 1.380692] davinci_mdio 4a101000.mdio: davinci mdio revision 1.6, bus freq 1000000 [ 1.388722] davinci_mdio 4a101000.mdio: detected phy mask fffffffe [ 1.399374] libphy: 4a101000.mdio: probed [ 1.403814] davinci_mdio 4a101000.mdio: phy[0]: device 4a101000.mdio:00, driver SMSC LAN8710/LAN8720 [ 1.414871] cpsw 4a100000.ethernet: Detected MACID = 68:9e:19:57:77:f3 [ 1.422248] cpsw 4a100000.ethernet: initialized cpsw ale version 1.4 [ 1.428889] cpsw 4a100000.ethernet: ALE Table size 1024 [ 1.434542] cpsw 4a100000.ethernet: cpts: overflow check period 500 (jiffies) [ 1.445146] i2c /dev entries driver [ 1.452690] omap_hsmmc 48060000.mmc: Got CD GPIO [ 1.571497] ledtrig-cpu: registered to indicate activity on CPUs [ 1.580846] oprofile: using arm/armv7 [ 1.585400] Initializing XFRM netlink socket [ 1.590306] NET: Registered protocol family 10 [ 1.602723] Segment Routing with IPv6 [ 1.606684] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver [ 1.614838] NET: Registered protocol family 17 [ 1.619557] NET: Registered protocol family 15 [ 1.624722] Key type dns_resolver registered [ 1.629351] omap_voltage_late_init: Voltage driver support not added [ 1.636104] sr_dev_init: No voltage domain specified for smartreflex0. Cannot initialize [ 1.644608] sr_dev_init: No voltage domain specified for smartreflex1. Cannot initialize [ 1.653524] ThumbEE CPU extension supported. [ 1.658007] Registering SWP/SWPB emulation handler [ 1.663099] SmartReflex Class3 initialized [ 1.701671] mmc0: host does not support reading read-only switch, assuming write-enable [ 1.713670] mmc0: new high speed SDHC card at address aaaa [ 1.721961] mmcblk0: mmc0:aaaa SL08G 7.40 GiB [ 1.731624] mmcblk0: p1 p2 [ 1.744292] random: fast init done [ 1.755440] mmc1: new high speed MMC card at address 0001 [ 1.763168] mmcblk1: mmc1:0001 MMC04G 3.66 GiB [ 1.769208] mmcblk1boot0: mmc1:0001 MMC04G partition 1 1.00 MiB [ 1.776723] mmcblk1boot1: mmc1:0001 MMC04G partition 2 1.00 MiB [ 1.784677] mmcblk1rpmb: mmc1:0001 MMC04G partition 3 128 KiB [ 1.795501] mmcblk1: p1 [ 1.810817] tps65217 0-0024: TPS65217 ID 0xe version 1.2 [ 1.817329] omap_i2c 44e0b000.i2c: bus 0 rev0.11 at 400 kHz [ 1.827080] omap_i2c 4819c000.i2c: bus 2 rev0.11 at 100 kHz [ 1.834579] hctosys: unable to open rtc device (rtc0) [ 1.839873] sr_init: No PMIC hook to init smartreflex [ 1.845541] sr_init: platform driver register failed for SR [ 1.932384] EXT4-fs (mmcblk0p2): recovery complete [ 1.940401] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null) [ 1.949174] VFS: Mounted root (ext4 filesystem) on device 179:2. [ 1.963847] devtmpfs: mounted [ 1.969162] Freeing unused kernel memory: 1024K [ 2.093204] EXT4-fs (mmcblk0p2): re-mounted. Opts: data=ordered Starting syslogd: OK Starting klogd: OK Initializing random number generator... [ 2.378602] random: dd: uninitialized urandom read (512 bytes read) done. Starting network: OK OK Welcome to Buildroot buildroot login:
Then I checked if I got the USB Interface for Beaglebone using the following the command:
# ifconfig -a
eth0 Link encap:Ethernet HWaddr 68:9E:19:57:77:F3
BROADCAST MULTICAST MTU:1500 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
Interrupt:45
lo Link encap:Local Loopback
inet addr:127.0.0.1 Mask:255.0.0.0
inet6 addr: ::1/128 Scope:Host
UP LOOPBACK RUNNING MTU:65536 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
sit0 Link encap:IPv6-in-IPv4
NOARP MTU:1480 Metric:1
RX packets:0 errors:0 dropped:0 overruns:0 frame:0
TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:0 (0.0 B)
I am unable to understand Why my kernel can detect the ethernet but, not the USB port?
What kernel configurations or other configurations are required to detect the USB port for buildroot?