This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Peripheral Address Errors in "hardware.h"

I believe these are mistakes in this header file. Perhaps someone would like to correct them. Can't say I wouldn't make them if this file was my responsibility.

#include <asm-arm/arch-davinci/hardware.h>

#define DM3XX_TIMER2_BASE       (0x01C20800) // 0x01C2 1C00 in datasheet.

#define DM365_TIMER3_BASE       (0x01C23800) // This is the address for timer 4 in the datasheet. Timer 3 should be 0x01C2 0800.

No definition for timer 4.