Tool/software: Linux
1、What does each line of screen printing on the chip surface mean? Is the red line marked for batch information?
2.At present, our company's production line feedback has the following failure phenomena, whether it is related to chip anomalies?
1)Program can not be downloaded, JTAG can not be connected, test power supply voltage is normal, FLASH no load signal
2)The download program is successful, you can't read back version information, test with JTAG, the connection is not smooth, you can't configure DDRAM, test the power supply voltage is normal.
3)Download the program successfully, can not read back version information, test with JTAG, the program loaded into DDRAM and run away
4)The download program is successful, the version information can be read back, and the program runs normally.