Part Number: 66AK2E05
Tool/software: TI C/C++ Compiler
Hi ,
I would like to setup own compilation environment without ccs for being able to cross compile linux process binary for arm A15 cores . This should be done as part of automated building procedure
on Linux (CentOS 7) machine
Typically I would need the following (??)
SYSROOT, TOOLCHAIN
So question is if within keystone k2e sdk (ti-processor-sdk-linux-k2e-evm-05.00.00.15) these are the correct paths:
- linux-devkit/sysroots/x86_64-arago-linux/ or
- linux-devkit/sysroots/armv7ahf-neon-linux-gnueabi or none of these 2 ?
Then to "override" the host machine compilation tools/environment for example like this:
make CC="arm-linux-gnueabihf-gcc --sysroot=$SYSROOT -I=/usr/include -L=/usr/lib"
MOreover how can we setup as such for DSP core for TI-RTOS ?