Part Number: AM4379
Other Parts Discussed in Thread: TPS51200
Tool/software: Linux
Hi,
we developed a own AM437x board, which can be booted from sd-card, network or qspi.
Booting from sd-card or network works fine. When I boot from sd card and flash with ubiformat -f the qspi flash it looks like everything works fine.
After trying to boot from flash spl and uboot comes up, but during booting the kernel there are major flauts, wichs stopps boot process.
Sine I have a similar board, which I can boot up from the flash with the same image, it has to be something with the hardware I guess.
But I had a look at the signals of the qspi with a oscilloscope and they look ok.
So do you have any idea, what might go wrong? Or is there a way to check, wheter the image flashed successfully? Some ubi command to read back the image and compare it?
Best Regards,
Stefan