This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM365 Bootup Problem

Hi.,

i am trying to Bring up custom board with DM365 processor and the schematic is almost same as DM365evm, The nand , DDR  same. xcluded ethernet and some components.

i am using  TI UBL Version: 1.50 from DVSDK_3_10_00 3_10_00_19.

UBL an uboot sucessufully loaded in to NAND and i am using loady command to load the  kernel.

after loading it strucks in Starting Kernel.....

if i used the pre built binires then it gets restart in .............done, booting Linux.

The log :

TI UBL Version: 1.50                                                                                                     
Booting Catalog Boot Loader                                                                                              
BootMode = NAND                                                                                                          
Starting NAND Copy...                                                                                                    
Valid magicnum, 0xA1ACED66, found in block 0x00000019.                                                                   
   DONE                                                                                                                  
Jumping to entry point at 0x81080000.                                                                                    
                                                                                                                         
                                                                                                                         
U-Boot 2009.03 (Dec 01 2010 - 17:30:39)                                                                                  
                                                                                                                         
I2C:   ready                                                                                                             
DRAM:  128 MB                                                                                                            
NAND:  NAND device: Manufacturer ID: 0x2c, Chip ID: 0xd3 (Micron NAND 1GiB 3,3V 8-bit)                                   
Bad block table found at page 262080, version 0x01                                                                       
Bad block table found at page 262016, version 0x01                                                                       
nand_bbt: ECC error while reading bad block table  

1024 MiB

NAND device: Manufacturer ID: 0x2c, Chip ID: 0xd3 (Micron NAND 1GiB 3,3V 8-bit)                                   
Bad block table found at page 262080, version 0x01                                                                       
Bad block table found at page 262016, version 0x01                                                                       
nand_bbt: ECC error while reading bad block table        
                                                                      
1024 MiB                                                                                                                 
*** Warning - bad CRC or NAND, using default environment                                                                 
                                                                                                                         
In:    serial                                                                                                            
Out:   serial                                                                                                            
Err:   serial                                                                                                            
Hit any key to stop autoboot:  0                                                                                         
DM365 EVM > loady 0x80700000
## Ready for binary (ymodem) download to 0x80700000 at 115200 bps...                                                     
C/0(STX)/0(CAN) packets, 3 retries
## Total Size      = 0x00214958 = 2181464 Bytes
DM365 EVM > bootm 0x80700000
 ## Booting kernel from Legacy Image at 80700000 ...
   Image Name:   Linux-2.6.32-rc2-davinci1
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    2181400 Bytes =  2.1 MB
   Load Address: 80008000
   Entry Point:  80008000
   Verifying Checksum ... OK
   Loading Kernel Image ... OK
OK

Sarting kernel ...

 

The printenv

 

DM365 EVM > printenv
bootargs=mem=60M console=ttyS0,115200n8 root=/dev/mtdblock4 rw rootfstype=jffs2 ip=off video=davincifb:vid0=OFF:vid1=OFF:osd0=720x576x16,2025K dm365_imp.oper_mode=0
bootcmd=nboot.e 0x80700000 0 0x1000000;bootm
bootdelay=4
baudrate=115200
bootfile="uImage"
stdin=serial
stdout=serial
stderr=serial
ver=U-Boot 2009.03 (Dec 01 2010 - 17:30:39)

Environment size: 341/262140 bytes
DM365 EVM >